Consulter la FAQ



Spare parts list for ACRD1XX, and ACRD2XX
1 /2"ODM X 5 / 8 " ODF EXTENDED, r410a 3 TON - SPARE PART 0.656 160.0 ...
How to configure the SRC 5,6,8 & 10 KVA UPS Models External Battery Packs using the LCD display
All SRC models , All Serial ... Resolution : 1 . Press the ... 5 . Enter the ... ... of battery) x (total number ... Example 1 : If there ... ... series(for 5 KVA), ... is 100 AH x 16 pcs= ... The 80ah inside the table is the default setting for 5kva/6kva ( 1 EXB: 16pcs of 5ah battery) The default setting for 8kva is 140ah ( 1 EXB: 20pcs of 7ah battery) The default setting for 10kva is 180ah ( 1 EXB: 20pcs of 9ah battery).
How to enable .NET 2.0 on Windows 8.x and 10
Windows 8 . x and 10 ... .Net 2.0 is not pre- installed as part of the OS ... You will need to install the .Net 3.5 1 . Open up the control panel. (Right click start - then click control panel) ... 5 . You should see .NET Framework 3.5 (includes .NET ... Framework 3.5 and click ok. Windows will proceed to install the service (downloading it from windows update if necessary). ... 2.0 you can now install PowerChute Personal Edition 3.0.2
“Failed dependency error on terminal” during PowerChute Business Edition 8.0.1, 9.0.x, 9.1.x and 9.2.x installation on Red Hat Enterprise Linux 6.x, 7.x and Oracle Linux 7.3
The installation requires 32- ... ... .1. x , ... versions 6. x and 7. x ... x64 Operating System installation . 1 . Registered Red ... ... "glibc- x .xx- x .xx. ... ... -freebl- x .xx. x - x .xxx. ... ... the CD of one of the following ... ... * glibc- x .xx- x .xx. ... -freebl- x .xx. x - x .xxx. ... (Replace x with the relevant ...
Network Air FM unit spare parts list
875-1059/875-1057a TXV 5 / 8 " X 1 - 1 / 8 " R22 - (FM NEW ACFM MODELS )
Symmetra LX Seismic Anchoring for Tower Models
( 8 ) 812-0011a - 5 /16" 18 thread count x 1 " long Bolts used to attach L-bracket ...
NetBotz 750 | What parts come with the NetBotz 750?
1 NetBotz Rack Monitor 750 1 2 Wireless Coordinator ... (nbwc100u) 1 3 Brackets for ... , M4 x 8 4 5 2-position ... terminal block plug 1 8 tie wraps, 203 mm ( 8 in) 2 ...
Video: Data Center Expert | Desktop Client Requirements, Download, & Installation
... to download and install the client application ... Resolution : ... discusses downloading and installing the Desktop Client ... ... PC with a 1 -GHz or ... 7, Windows 8 , or Windows ... At least 1 GB of RAM Screen resolution should be set ... at least 1024 x 768. 1 ) Open the ... 5 ) Run the downloaded execuatble file and follow the on-screen instructions. 6) Once the installation completes, you can launch to the Desktop Client using the Desktop Icon (if done during installation ) or the Start Menu Option for StruxureWare Data Center Expert #.#.#.
What size is the threaded rod of the Ladder Stacking Kit, and will ours fit on other manufacturer's ladder?
Customers need to know the spec of the threaded rod for installation design. Resolution : ... The threaded rod has 5 / 8 "-11 coarse threads. ... The Ladder Stacking Kit will mount onto a ladder rail with the maximum dimensions of 1 1 /4" tall x 1 /2" thick. ... This kit is then used to suspend another ladder underneath the first one .
Why are the red outlet LEDs always scrolling on Rack PDU models AP7855 or AP7867?
... Metered Rack PDU models , specifically Scenario 1 : ... default settings should resolve this issue. Resolution ... value to known one . ... be greater than 5 A) on L 1 Outlet 2. ... if the connected load is 8 A then enter 80). ... If the user does not have the ability to connect a known load on L 1 outlet 2 then follow this second procedure. ... If the outlet load still reads high load values by an amount of, say, X amps then record this value. ... Provide previous recorded value X as negative and multiply by 10 (-10x).


Résultats 1 - 10 de 98

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.