Browse FAQs

PowerChute Business Edition version 10.x fails to install on VMware vMA with error "System Locale is set to C"

Published date: 21 April 2020

Issue:
PowerChute Business Edition fails to install on VMware vMA with error "System Locale is set to C. Please reset System Locale"



Product:
PowerChute Business Edition 10.x

Environment:
VMware vMA  6.x

Cause:
Profile set to the wrong locale.

Solution:
Change the locale of the profile.

Open the profile file using the following command: sudo vi /etc/profile

Add one of the following to the end of the profile file:

 #English
export LC_ALL=en_US.utf8
export LANG=en_US.utf8
export LANGUAGE=en_US.utf8

#Chinese
export LC_ALL=zh_CN.utf8
export LANG=zh_CN.utf8
export LANGUAGE=zh_CN.utf8

 #Japanese
export LC_ALL=ja_JP.utf8

export LANG=ja_JP.utf8
export LANGUAGE=ja_JP.utf8

Remove any lines in the profile file that contain “export LANG=C.utf8”.

Reboot the vMA

Confirm that the system locale has changed by entering the command: Locale

NOTE: If you are not familiar with using vi editor you can copy the file to a Windows system and edit the file with a text editor. Then copy the file back.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.