Cause:
Leak rope integration into Botzware does not detect the location or zone along the cable where the leak is detected.
Resolution:
The Leak Rope sensor and extension acts like a dry contact. It either detects conductivity or does not. The NetBotz appliance has no code in it to detect where on the cable or it's extensions that it has detected a leak.
If it is critical to know where exactly a leak has been detected, it is suggested that you use spot leak sensors instead of a rope leak.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.