What is the range for Netbotz wireless sensor range?
Published date:
17 July 2020
Issue:
What is the range for Netbotz wireless sensor range?
Product Line:
Netbotz Appliance
Environment:
Netbotz Appliance Version
Cause:
Expected range of NetBotz wireless sensors.
Resolution:
Supported devices on the NetBotz wireless network
The Wireless Temperature Sensor is always configured as an End Device in your wireless sensor network.
The following wireless devices can be configured as a Coordinator or Router:
Sensor Name Range Part Number
NetBotz USB Coordinator & Router 100 ft-line of sight NBWC100U
NetBotz Wireless Sensor Pod 180 100 ft-line of sight NBPD0180
The following wireless devices can be configured as an End Device:
Sensor Name Range Part Number
NetBotz Temperature Sensor 100 ft -line of sight NBWS100T/ NBWS100H
NetBotz Wireless Sensor Pod 180 100 ft -line of sight NBPD0180
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.