Browse FAQs

How to access User menu on a EcoBreeze Expansion Module.

Published date: 30 March 2020

                                                                                                                                                        

Issue:   
This article contains information on how to access User menu on a EcoBreeze Expansion Module.

Product line:
ACEC200, ACEC201. 

Environment:  
All serial numbers. 

Cause:  
Install. 

Resolution:    

This menu can be accessed/viewed from any point within the User menu by pressing the UP+DOWN buttons for about 4 seconds. The first variable displayed is rI00 (evaporation pressure). rI00 to rI15 and PA menus are accessible. 

• Press the ENTER button to view the relative value. 

• Press the ENTER button again to come back to the variable list. 

• Use the UP/DOWN button to scroll through the list of module variables. 

If the DOWN button is pressed while the rI00 variable is being displayed, the device requests the PA password to access Installer menu. The only variable which can be modified from this level is PA, the password.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.