What are the electrical specifications of the power supply for ACF600?
Published date:
12 August 2020
Issue:
Customers may need electrical specifications for the ACF600 power supply.
Product Line:
NetShelter AV
Environment:
ACF600 all versions and serial ranges.
Cause:
Review of the electrical specifications of the ACF600 power supply.
Important Note: This unit should only be used with regulated power supplies. If not using a regulated power supply and using an unregulated adjustable voltage power supply such as the PS-300 or PS-500, the power supply should then possibly require a setting of 9V, although this is not optimal. The issue is that often times unregulated power supplies will supply higher voltage when not under load or under a light load. Higher voltage will not damage the unit, it simply will not perform within the specifications. Connection: 2-Pin FastWire Power System (Ensure proper polarity - Tip to +) Voltage: 12V DC ***See “Important Note” above*** Current - Amps: Output Rated at 2 Amps (Max)