Browse FAQs
Serial Terminal Connection Parameters for all NetBotz Appliances When connecting to a Netbotz appliance or a NetBotz Central via a serial cable, the terminal settings must be set to: 38400 and 8-N-1 When connecting to a models 300, 303, 310, or 400, you must use a standard serial cable, such as the kind used to connect a modem to a PC. When connecting to models 320, 420 or 500, you must use a NULL modem cable.
When connecting to models 355, 455, 550, 570 or similar version 3 Netbotz, you must use a USB A-B cable. The NetBotz 200 uses a Null Modem cable and a baud rate of 9600. NOTE: When connecting to a NetBotz Central, you must use a NULL modem cable.