Browse FAQs



Smart-UPS SRC 5k, 6k, 8k and 10 KVA FAQ
A: In addition to the 1 + 1 Parallel redundancy system, the Customer can also look into a service bypass panel which will ...
Does the NTP need to be configured on the Galaxy VS internal NMC and the optional AP9644 NMC for all parallel or single Galaxy VS?
Issue: Does the NTP need to be configured on the Galaxy VS internal NMC and the optional AP9644 NMC for all parallel or single Galaxy VS
Does the NTP need to be configured on all NMCs for all parallel Galaxy VS?
Resolution: Ensure that only one network management interface in the entire UPS system ( single or parallel ) is set to synchronize time.
Symmetra PX 250/500; AP9635; Flood of RTC Time adjusted values in the logs
... -2015 17:12:53 006 46933 Info RTC Time adjusted value Parallel UPS 1 2 02-26-2015 17: ...
Connecting UPS Outputs Together (Paralleling UPS)
Paralleling output power of our units to one single phase distribution panel is not an option.
PowerChute Network Shutdown reports "Available runtime has been exceeded".
... and event actions are carried out even if it occurs on a single UPS in a Redundant or Parallel UPS configuration.
EPW9 APC ISX EPO Actuator Switch; product specifications and installation
The cascading cables parallel the contacts of actuator switch so that any one can EPO all connected devices (up to eight in total) ...
What's the difference between seismic Zone 4 maps and High Seismic Area maps? Can one be substituted for the other? Which cabinet should I choose?
An example of such tailoring is given by the evolution of the UBC since its adaptation of a pair of 1976 contour maps.
Can EPO Circuits be Wired in Parallel?
Independant poles of an EPO ( single action, multi-pole) switch must be run to each UPS.


Results 1 - 10 of 31

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.