Consulter la FAQ



Symmetra LX Spare Parts List
Symmetra LX Communications Card - SYAFSU15 Symmetra LX 13 U replacement door - SYAFSU2
In the NetShelter WX 6U Vertical cabinet, is the 2U UPS Mounting Bracket adjustable to 1U for a 1U UPS?
Issue: It is unknown whether a 1 U UPS can use the 2 U mounting rail .
In the NetShelter WX 6U Vertical cabinet, must the included 2U UPS Mounting Bracket be used?
ar106v, ar106vi, mounting, rail , rails , bracket, brackets,
Can vertical cable managers or 0U accessory rails be installed in the front and rear of a NetShelter SX cabinet?
Cause: Owner's Manuals show cable managers and 0 U accessory rails installed in specific areas of the cabinet.
Are there any functional differences between the NetShelter HS and SX?
In the NetShelter SX there are some 0 U mounting spaces behind the vertical rails of the frame.
Do the 800 mm wide NetShelter SV cabinets have 1U rackmount spaces in the vertical mounting rails?
Cause: It appears there may be a 1 U punch out in the vertical mounting rails .
What's the vertical mounting rail depth for the NetShelter SX cabinets?
The vertical mounting rails of the NetShelter are marked with numbered U -spaces on both the front and back.
Can a 3rd party UPS be installed in the ar106v or ar106vi?
The NetShelter WX 6 U Vertical cabinets have a mounting bracket for a 2 U UPS. ... When shipping with a 3rd party UPS installed, the manufacturer must validate that the 3rd party UPS can ship installed using their rail kit(s), without disconnecting in transit.
How many finger-style vertical cable managers are required to fully populate one rail in a NetShelter cabinet?
Resolution: For all of the following skus, quantity 1 contains two cable managers that will populate one (1) vertical rail height:


Résultats 1 - 10 de 71

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.