Browse FAQs



What is the maximum number of rack access cards that can be configured in a version 3 NetBotz appliance for use with the rack access pod 170?
When using StruxureWare Data Center Expert to configure multiple NetBotz appliances, the limit in this system is also 200 cards and again all cards ...
Why does ISX Manager/StruxureWare Central display the incorrect Kilowatt value when utilizing the Physical Layout or ISX Operations feature for my Metered/Switched Rack PDU product?
... or ISX/ StruxureWare Operations tools from my Metered or Switched Rack PDU. ISX Operations StruxureWare Data Center Operations ... and AP88XX Metered Rack PDUs ... Metered By Outlet Rack PDUs ... and AP86XX Metered Rack PDUs ISX or StruxureWare Operations - All Versions ... Physical Layout or StruxureWare Central Operations to display the ... ... (AP79XX) Rack PDU's as well ... ) that have 3 .X. ... ISX Manager or StruxureWare Central via SNMP ... Physical Layout or StruxureWare Operations tool. ... /or Switched Rack PDU and inline ... Alternatively, these values can be changed via SNMP on most prior rpdu APP revisions.
Data Center Expert | How do hardware and software support contracts work?
Cause: StruxureWare Data Center Expert appliances come with 2 years of factory hardware warranty and no
StruxureWare Data Center Expert v7.4.2 is no longer available
Resolution You must have a valid support contract to receive the software update.
Why doesn't StruxureWare or ISX Manager's mass configuration feature update or show password credentials on APC Network Management Card devices?
... ISX Manager or StruxureWare may not work ... ... Metered/Switched Rack PDUs (AP78XX ... AP79XX), Rack Automatic Transfer Switches ... ap9340, NetBotz 200 ) ... Metered/Switched Rack PDUs (AP86XX ... In general, with firmware versions v 3 .X.X and v5.X.X, the config.ini ... The config.ini file could be manually configured outside of ISX Manager to include the password using the information from the [SystemUserManager] section above. ... If you have ISX Central or StruxureWare Data Center Expert, this should not be an issue.
Video: Data Center Expert | Desktop Client Requirements, Download, & Installation
The StruxureWare Data Center Expert Desktop Client (console) is a stand -alone Java application that runs on systems that meet the following ...
Can StruxureWare Data Center Expert be configured to alert for NetBotz 3xx, 4xx, and 5xx devices?
Please note that this is different than the NetBotz Rack Access AP9361, NetBotz 200 , or NetBotz 250 which are monitored using SNMP.
NetBotz v3 | How do I configure location settings?
StruxureWare Data Center Expert will only pull in the main location field of the Sensor Pods, Rack Access Pods, and wireless devices to ...
Application Version within StruxureWare Data Center Expert client does not update after upgrading devices to AOS 6.4.6 and newer
... 2 include (but are not limited to): 2G Metered/Switched Rack PDUs (AP84XX, AP86XX, AP88XX, AP89XX ...


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.