Browse FAQs

NetBotz 250 | Network Port Light Indicators

Published date: 04 September 2019

Issue:
   Description of the Network Port lights (Link/Status) on NetBotz 250

Product Line:
   NetBotz Rack Monitor 250 (NBRK0250)

Environment:
   NetBotz Rack Monitor 250 (all versions)

Resolution:

Link (10/100) LED
The LED on the right of any network port indicates the network status.
 
Condition Description
Off One or more of the following situations exist:
  • The Rack Monitor 250 is not receiving input power.
  • The cable that connects the Rack Monitor 250 to the network is disconnected or not functioning properly.
  • The Rack Monitor 250 is turned off or not operating correctly. It may need to be repaired or replaced. Contact Customer Support at www.apc.com/support.
Solid Green The Rack Monitor 250 is connected to a network operating at 10 Megabits per second (Mbps).
Solid Orange The Rack Monitor 250 is connected to a network operating at 100 Mbps.
Flashing Green The Rack Monitor 250 is receiving or transmitting data packets at 10 Mbps.
Flashing Orange The Rack Monitor 250 is receicing or transmitting data packets at 100 Mbps.

Status LED
The LED on the left side of any network port indicates the status of the appliance.
 
Condition Description
Off One of the following situations exists:
  • The Rack Monitor 250 is not receiving input power.
  • The Rack Monitor 250 is not operating properly. It may need to be repaired or replaced. Contact Customer Support at www.apc.com/support.
Solid Green The Rack Monitor 250 has valid TCP/IP settings.
Flashing Green The Rack Monitor 250 does not have valid TCP/IP settings.1
Flashing Orange The Rack Monitor 250 is making BOOTP requests.
Rapidly Flashing Green A user initated a LED blink test from the user interface.
Alternately flashing green and orange If the LED is flashing slowly, the Rack Monitor 250 is making DHCP requests.1
If the LED is flashing rapidly, the Rack Monitor 250 is starting up.

If you do not use BOOTP or DHCP server, the network settings will need to be configured manually.  Instructions for manually configuring TCP/IP settings can be found in knowledge base FA381239.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.