APC Din Rail/Panel Mount UPS and External Batteries
Published date:
27 August 2020
Issue: The installation guide for for the APC Din Rail/Panel Mount UPS Battery Replacement specifies how to connect an External Battery to the UPS.
Product Range: SUA500PDR-S, SUA500PDR-H
Resolution:
These UPS models do not have extended run capability. The installation guide refers to the feature that allows connecting the RBC externally to the UPS. The purpose for attaching a battery externally to the UPS is to accommodate installation requirements for specific applications that require the UPS to be enclosed with control devices in an 'air tight' enclosure. Batteries should not be inside this type of enclosure. With the chassis design on SUA500PDR models, the associated battery can be mounted in a separate appropriately vented enclosure by using the extended length cable included with the battery.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.