What are the hole sizes and dimensions of the AR8395 copper bus bar?
Published date:
05 August 2019
Issue:
A customer wants to use 2-hole lugs on the ground bar
Product Line:
NetShelter Bus Bar
Environment:
AR8395
Cause:
Grounding / bonding is required
Resolution:
The AR8395 has the following holes available:
47 holes threaded #10-32, spaced 18 cm center to center.
25 holes at 5.5 cm and 9 holes at 7.9 cm, spaced at 25 cm center to center.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.