Issue:
Can I run cables over the SC? If so, how many?
Product line:
ACSC1XX.
Environment:
All Serial Numbers.
Cause:
FAQ.
Resolution:
Yes, there is a cable support bridge trough available as an accessory (ACAC10021). You will need (2) per SC unit to carry
both data and power cables across the unit. Approximately 80 CAT5 cables or 8 power whips fit into a trough.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.