Output relay state upon boot up of a Netbotz version 3 appliance.
Published date:
17 July 2020
Issue:
Output relay state upon boot up of a Netbotz version 3 appliance.
Product Line:
NetBotz
Environment:
Netbotz Version 3 output relay.
Cause:
Relays have a default state defined at startup. This is defined for factory defined switches and buttons as well as for custom created switches and buttons. Upon a reboot of the Netbotz appliance, the relays will go back to their default state. If there is an alert that is configured to trigger a state change on one of these buttons or switches, the state will then change as configured.
Resolution:
This is working s designed.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.