Details Returned from Compaq Devices via Advanced Device Crawlers
Published date:
17 July 2020
Issue:
Details Returned from Compaq Devices via Advanced Device Crawler
Product Line:
NetBotz
Environment:
NetBotz version 2 Advanced Device Crawlers.
Cause:
The following information can be queried via Advanced Device Crawlers for Compaq systems assuming the Compaq DDF (Device Definition File) is installed on the NetBotz appliance and the Compaq system is SNMP enabled. Please note that not all information listed below is available on all Compaq models.
Resolution:
Description
Overall Thermal Condition
Thermal Degraded Action
Temperature Status
Fan Status
CPU Fan Status
Fan Present
Fan Type
Fan Speed
Fan Redundancy
Fan Condition
Power Supply Present
Power Supply Condition
Power Supply Status
Power Supply Main Voltage
Power Supply Capacity Currently Used
Power Supply Maximum Capacity
Power Supply Redundancy State
Power Converter Module Present
Power Converter Module Slot
Power Converter Module Socket
Power Converter Module Redundant
Power Converter Redundant Module Group ID
Power Converter Module Condition
Storage System Box Type
Storage System Box Condition
Storage System Fan Status
Storage System Temperature Status
Storage System Side Panel Status
Storage System Fault Tolerant Power Supply Status
Storage System Box Placement
Storage System Connection Type
Storage System Chassis Overall Condition
Storage System Power Supply Condition
Storage System Fan Condition
Storage System Temperature Condition
Storage System Fibre Channel Array Controller Condition
Storage System Fibre Channel Array Logical Drive Condition
Storage System Fibre Channel Array Physical Drive Condition
Storage System Backplane Condition
Storage System Power Supply Status
Storage system Power Supply UPS Status
Storage System Power Supply Condition
Storage System Fan Module Status
Storage system Fan Module Condition
Storage System Temperature Sensor Status
Storage System Temperature Sensor Condition
Storage System Temperature Sensor Value
Storage System Backplane Condition
Storage System Backplane Fan Status
Storage System Backplane Temperature Status
Storage System Backplane Fault Tolerant Power Supply Status
RAID Storage System Status
RAID Storage System Condition
UPS Line Status
UPS Name (type)
UPS Battery Time Remaining (minutes), (-1 = not supported)
UPS Alarm Text
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.