Browse FAQs

OID Information for External Humidity Sensor on Version 1 Appliances

Published date: 10 December 2019

Issue:

OID Information for External Humidity Sensor on Version 1 Appliances

Product Line:

NetBotz

Environment:

NetBotz version 1 and SNMP

Cause:

The OID information for the NetBotz External Humidity Sensor is all in the published MIB under:
iso.org.dod.internet.private.enterprises.netBotz.ExpPortTable.expPortEntry.expPort-ext-humi

Resolution:

The OID information for the NetBotz External Humidity Sensor is all in the published MIB, under iso.org.dod.internet.private.enterprises.netBotz.ExpPortTable.expPortEntry.expPort-ext-humi.

The OIDs map to:
.1.3.6.1.4.1.5528.31.1.80.1.0 (for External port 1)
.1.3.6.1.4.1.5528.31.1.80.2.0 (for External port 2)
.1.3.6.1.4.1.5528.31.1.80.3.0 (for External port 3)
.1.3.6.1.4.1.5528.31.1.80.4.0 (for External port 4)
.1.3.6.1.4.1.5528.31.1.80.5.0 (for External port 5)
.1.3.6.1.4.1.5528.31.1.80.6.0 (for External port 6)
.1.3.6.1.4.1.5528.31.1.80.7.0 (for External port 7)


Please note that version 1 NetBotz are no longer supported.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.