Technical FAQs

Ask a Question

How to Update the Main Firmware (BARROW) Controller on my ACPA4000

 
Issue:
How to update the firmware on an ACPA4000 Barrow controller.
Product line: 
ACPA4000
Environment: 
All Product models, all serial numbers 

Cause: 
Install, Firmware Upgrade
Resolution:
This document will explain how to install main firmware on an ACPA400 cooling unit from APC. This firmware is need when a new board is being installed, or the unit appears to be having technical issue.
Was this helpful?
What can we do to improve the information ?