Technical FAQs

Ask a Question

Video: Troubleshooting no communication between UPS and PowerChute Business Edition
Issue: No Communication with UPS Product Line: PowerChute Business Edition   Environment: All supported OS Cause: There are many possible causes....
Can I use a NetBotz NBPD0165 camera pod with older NetBotz appliances?
Issue: Can I use a NetBotz NBPD0165 camera pod with older NetBotz appliances? Product Line: NetBotz Environment: NetBotz cameras Cause: NetBotz has...
Why is my NetBotz 750 browser window hanging after upgrading the firmware from 5.0.1?
Issue: After upgrading NetBotz 750 firmware, the upgrade appears to hang. Product Line: NetBotz Environment: NetBotz 750 firmware upgrade. Cause:...
How do I serially connect to the NetBotz 750?
Issue: How do I serially connect to the NetBotz 750? Product Line: NetBotz Environment: NetBotz 750 serial port configuration and driver Cause: The...
NetBotz 4.6.3 e-mail "From" address shows as "Unknown"
Issue: NetBotz 4.6.3 e-mail "From" address shows as "Unknown" Product Line: NetBotz Environment: NetBotz version 4.6.3 firmware Cause: A change was...
Java Cryptography Extension requirement for SNMPv3 configuration in PowerChute Network Shutdown and PowerChute Business Edition
Issue: In certain geographies it is necessary to install the Java Cryptography Extension to use privacy protocols AES-192 or AES-256 in the PowerChute...
International Connectors & Country Comparison Reference Chart
Issue: International Connectors & Country Cross Reference Chart Product Line: N/A Environment: N/A Cause / Resolution:   Country Follows the Connectors...
What is the definition of the shutdown types in PowerChute Business Edition?
Issue: Need to know the different shutdown types in PowerChute Business Edition. Product Line: PowerChute Business Edition Environment: All supported...
Video: How to run PowerChute Network Shutdown setup wizard & configure for VMware ESXi hosts and vCenter Server
Issue: Need to setup PowerChute Network Shutdown for VMware ESXi hosts and vCenter Server. Product: PowerChute Network Shutdown v4.2 Environment:...
UPS fails to automatically power on if AC Power is restored before PowerChute Network Shutdown has issued a UPS/Outlet Group turn off command.
Issue: After PowerChute Network Shutdown has shut down Virtual Machines and Hosts, when AC Power is restored the UPS does not return power to the...
Results 1 - 10 of 100