Cause: A customer may want to install split doors onto the front of a NetShelter SX cabinet.
Resolution :
Rear split doors can be installed onto the front of a NetShelter SX, VX and SV cabinets.
A replacement split door kit can be purchased or the existing split rear doors can be swapped to the front of the cabinet.
The replacement door kit includes all of the necessary hardware, including hinges.
The NetShelter one-piece front door may also be installed onto the rear of the cabinet.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.