Технические часто задаваемые вопросы



NetBotz 250 | Managing Wireless Sensor Networks (Coordinator/Router/Sensors)
1 ) Log into ... 4 ) Turn on ... ... turn on) one at a time ... label to each one by clicking on ... 1 ) Log into ... 4 ) Provide a ... 5) Enter the Extended Address ... 6) Enter a detailed location ... ... the Wireless Sensor Commission List. ... information within the Commission List to populate ... 1 ) Log into ... 4 ) Edit the thresholds as necessary and click Apply. ... 1 ) Log into the NetBotz 250 Web Interface. ... 1 ) Log into the NetBotz 250 Web Interface. ... 1 ) Log into the NetBotz 250 Web Interface. ... 4 ) Click on the name of the wireless sensor again.
Refrigerant charging table for a Uniflair Unit
1 . Open any ... 4 . After 24 hours, verify that no drop in pressure has occurred. ... 1 . Open any shut-off valves present in the system to ensure that all of the components will be evacuated. ... 4 . Wait for an hour and check vacuum level . The vacuum should not rise above 1500 microns; if vacuum level exceeds this level , check system for leaks. ... 4 . Charge to 80% of the calculated total. ... If the system is not ready for commissioning , then apply only a holding charge and record the amount charged.
How to navigate through an Network Air FM unit display
... and during the commissioning of the Modules ... ... work as a single System. ... Half capacity uses one compressor and half ... ... compressor (stage 1 ) in a ... ... or glycol line entering the heat exchanger ... event to one of the output ... ... °C ( 4 °F) ... Provide a unique name for each ... ... an input in one of the following ... ... , Expansion Module 1 , or Expansion ... ... > Expansion Module 1 > Module Config ... ... > Expansion Module 1 > Module Config ... ... tuned during the commissioning of each Module ... ... > Expansion Module 1 > Module Control ...
Network AIR FM Water Detected Shutdown Installation
Input: 1 of 4 (use enter then the down/up arrow to change the input number)
High Supply Temp Shutdown Installation on a NetworkAIR FM
: 1 of 4 (use enter then the down/up arrow to change the input number.
Is the NetShelter SX Zone 4 compliant? Are there Zone 4 compliance documents available for NetShelter SX or the mounting brackets?
UBC (Uniform Building Code) uses a Zone based map with Zones 1 thru 4 . UBC was replaced in 2000 by IBC ( ...
Galaxy VX; What is the Airflow and BTU heat dissipation?
... in m^3/hr and CFM for the same four load level (three at 30c and one at 40c) as the ...
What wires are protected by the various ProtectNet models?
PTEL2 and PTEL2R both protect wires 1 - 4 on an RJ11-, or wires 3-6 on an RJ45 cable
Uniflair Drain Line Connections
Connecting to the Drains The condensate water drains from the tray through a 1 1 / 4 ” flexible tube fitted in the unit.


Результаты 1 - 10 of 56

Не нашли то, что искали?

Обратитесь к нашей команде по обслуживанию клиентов для получения информации о технической поддержке, помощи в составлении претензий и другого.