Технические часто задаваемые вопросы



How do I recycle my UPS or UPS battery?
... , recycle, disposal, green, environment, eco, ecology, rbc, apcrbc
How to adjust the lens on the NetBotz Wallmount or the Camera Pod 160?
Issue: How to adjust the lens on the NetBotz Wallmount or the Camera Pod 160 ?
What kind of microphone can I use on a NetBotz appliance / Camera pod 160?
Issue: What kind of microphone can I use on a NetBotz appliance / Camera pod 160 ?
Can I use a NetBotz Camera Pod 160 nbpd0160 / nbpd0160a as a standalone appliance?
Issue: A customer may purchase a solution with the intension of using a NetBotz camera pod 160 on its own.
Maximum Size of SMS Message / Alert
The maximum size of an SMS text message sent via GSM is 160 single byte characters. Different carriers could potentially put lower limits.
"Slave Device Failure" message polling NetBotz device.
... will occur when polling the register assigned to the door switch on a camera pod 160 if the door switch is not connected.
Are spacers available for the leveling feet of NetShelter cabinets?
Please use ar7605 spacer kit. Each kit includes 160 pieces: (120 x 8mm) and (40 x 2.25mm)
Newly attached camera pod on a version 3 Netbotz appliance does not show time stamp.
This happens to both the newer camera pod 160 as well as the older version 2 camera pod 120.


Результаты 1 - 10 of 19

Не нашли то, что искали?

Обратитесь к нашей команде по обслуживанию клиентов для получения информации о технической поддержке, помощи в составлении претензий и другого.