Nutanix AHV: Prioritized VMs with 0 second Startup Duration are powered on
Published date:
05 October 2020
Issue: When a UPS critical event is cleared and PowerChute starts powering on VMs, any prioritized VMs with a 0 second Startup Duration are initially skipped and later powered on.
Environment:
PowerChute Network Shutdown configured with Nutanix Acropolis Hypervisor (AHV) support
Solution: This issue will be resolved in the next release of PowerChute Network Shutdown.
Alternatively, if your PowerChute configuration includes priority groups with a 0 second Startup Duration, you can disable VM Startup in PowerChute and power on VMs manually following a shutdown.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.