Browse FAQs



Batteries discharged to a low voltage in a single phase Symmetra frame
Single phase Symmetra battery ... 1 .) If ... in order to cool the battery and prevent the situation from ... ... and Symmetra RM units ship with caution ... ... Symmetra LX was designed with a total ... ... fresh battery ( greater than ~95 ... Once the system has fully charged the one fresh battery installed in the UPS, the discharged batteries can be installed in the system one at a time to be recharged.
DAC, Cancoil Installation Manual
Section 1 . Warranty and ... Section 1 . ... have been carefully designed to provide years of reliable performance ... stable, efficient year round operation for ... ... provided in the unit . DO ... SECTION OF THE UNIT . Unit Placement and Mounting ... unit should be securely ... structural base to prevent movement. ... clearance around the unit for proper servicing and preventative maintenance ... ... are based on 1 degree per 100 ... ... be sized to prevent excessive pressure drop ... ... a rate of 1 ” drop per ... ... vertical risers to prevent liquid and oil ... ... be sized to prevent excessive pressure drop ...
How to navigate through an Network Air FM unit display
... Network Air FM unit display. Only qualified service personnel should make ... ... MultiCool® ( chilled water) and ... ... point in the room . ... , then the cooling setpoint is used ... If the room temperature is 23 ... ... point of the room is 26° ... ... between the actual room dew point and the desired room dew ... to control the room environment or if ... ... work as a single System. ... Half capacity uses one compressor and half ... Rooms with small heat ... avoid over- cooling while dehumidifying. When the unit is in dehumidification ... ... the modes ( cooling , reheat, ...
Guidelines for installation of an acsc100, or acsc101
Room preparation During the design of the data ... . Ensure the room is insulated to ... room must be sealed ... The room should be thoroughly ... room should have a ... ... airflow for each unit supported. ... of heat per unit . Receiving the unit ... Your InRow SC unit has been factory tested and inspected prior to shipment. To ensure that you have received the unit in excellent condition, perform a careful inspection of the crating and the unit immediately upon receipt. ... If necessary, contact the APC technical service department at 1 -888-695-6500 for help in repairing or replacing damaged parts.
What are the operational conditions for an InRoom (Stulz) Unit
... (Stulz) Unit . The InRoom precision air conditioning units operate within the following ranges: Room Conditions: ... Frequency:60 Hz +/- 1 % Chilled water-/ cooling water pipes: ... Maximum equivalent length of piping between the cooling unit and the air cooled condenser: 60 m (200 ft) Maximum level difference between the condenser and the cooling unit : 5 m (16 ft) when the condenser is below the cooling unit ... Design Conditions ... Cooling fluid (DX): 30% Glycol ... Chilled water medium (CW): 0% Glycol
How does an FM use the dew point temperature to control humidity?
All Cooling Units . Product design . ... setpoint (use cooling setpoint if reheat ... ... point of the room is calculated from ... ... setpoint and the cooling setpoint. ... . If the room temperature is 74 ... point of the room is 48 F ... The humidifier demand is calculated as the difference between the actual room dew point and the desired room dew point divided by the sensitivity. ... There is one other note. ... COOL SETPOINT / DEHUMID SETPOINT = DEWPOINT HIGH LEVEL
Why is my ACRP excessively cycling?
Data Center Cooling ... to their basic design , loading, ... ... RP works to prevent this by giving ... ... supply air and cool setpoints both at ... ... the air the unit supplies to the ... The cool setpoint controls the ... ... relative to the cool setpoint). ... on the specific room configuration. Setting the cool setpoint between 72 ... and monitoring the unit performance, adjusting the cool and supply air ... ... will enable the unit to use the heater to help prevent excessive cycling ( ... under "configure unit " on the ... interface under the unit tab, then ... Installing blanking panels will definitely help prevent cycling of cool /warm air
What is the battery type and technology used in APC UPS Systems?
All APC Single Phase UPS Battery systems. ... All APC Single Phase UPS Battery systems. ... VRLA batteries are designed to recombine hydrogen and oxygen and emit only extremely small amounts of hydrogen under normal operating conditions. Normal room ventilation is sufficient to remove any hydrogen, so special ventilation is not required. ... The most common technology, termed “Absorbed Glass Mat (AGM) uses a highly porous, absorbent micro fiberglass mats that immobilize the electrolyte and prevents it from spilling.
What's the vertical mounting rail depth for the NetShelter SX cabinets?
A unique "captive" vertical rail design prevents the rail from dislodging during the adjustment process.
What is the maximum kW rating for the NetShelter SV?
The SV was not designed to have a removable roof or ... chimney, but as long as the cooling in the room is sufficient there ...


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.