자주 묻는 질문 찾아보기



Things To Consider When Upgrading or Downgrading a Network Management Card 2 (NMC2) Device between v5.X.X and v6.X.X
... Syslog settings, Paging settings, Remote Monitoring Service settings, Email settings, and Modbus settings (if applicable)
NetBotz Rack Monitor 250 Modbus Register Map Detail for MM_SENSOR_1_DISCRETE_STATE register/data point
... The NetBotz 250 Modbus Register Map references ... Environment Modbus TCP/serial ... ... and detail for Modbus users. ... may exist. Modbus 2 = Not Connected ... Smoke (nbes0307) - 0 = No Smoke, 1 = Smoke Detected, 2 = Not Connected Fluid (nbes0301) - 0 = No fluid, 1 = Fluid Fetected, 2 = Not Connected Vibration (nbes0306) - 0 = No Vibration, 1 = Vibration Detected, 2 = Not Connected
Netbotz | How do I monitor alarms using Modbus?
... on NetBotz using Modbus . Environment : ... NetBotz events using Modbus . Modbus output is not ... ... no way using Modbus to know the ... ... mimics the DCE modbus output and you ... ... , Enable the Modbus output on the “ Modbus Slave Communications” ... ... and older version 2 units does not ... ... example is using Modbus over TCP but ... ... using the ” Modbus Slave System” ... ... on the “ Modbus Slave System” ... ... pod as slave 2 : ... :Handle ( 2 ) 002 INT16 ... ... :Reader ( 2 ) 002 INT16 ... ... :Lock ( 2 ) 002 INT16 ...
Data Center Expert | Obtaining an SNMP or Modbus DDF for discovery of third-party devices
Environment 2 ) If the ... 2 ) SNMP DDF ... Modbus DDF: Device menu > Modbus Device Communication Settings > Device Definition Files > Add/Update Definitions > Local File > Browse > Select DDF XML > Open > Next > Check Box next to Name > Next > Finish. ... 2 ) Fill in the required information and follow the steps provided to provide additional required files.
Recommendations and Best Practices for the AP9622 Building Management Card
AP9622, building management card , BMS, modbus , jbus, rtu, troubleshooting, baud rate
How do I properly install/uninstall my SmartSlot accessory card into my UPS?
- ap9610/AP9613 Modbus /JBUS Building Management Card
RS-485 Converters for the UPS SmartSlot Building Management Card (AP9622)
Issue RS-485 Converter Compatibility for AP9622 Building Management Modbus /JBUS UPS SmartSlot card
Why is my AP9622 APC Building Management Card inaccessible after changing the slave ID?
AP9622, slave ID, slave address, 0x0d, building management card menu, menu, hyperterminal, modbus , RMA, rs- ...


결과 1 - 10 의 33

찾고 있는 내용을 찾을 수 없습니까?

기술 지원, 불만 사항에 대한 지원 등에 관한 정보를 얻으려면 고객팀에 문의하십시오.