자주 묻는 질문 찾아보기



Matrix-UPS emits a chirping sound after being on-battery or running a self-test
... test (either scheduled or through UPS start-up ), the Matrix-UPS will emit chirps for an interval of one minute ...
Video: Battery Installation of APC AV Power Conditioners with Battery Back-Up
... battery in a APC Power Conditioner with Battery Back-Up at first time start-up or following routine battery replacement.
NetBotz 750 | Accessing the Web User Interface (Web UI)
NOTE: The Web UI takes about six minutes to become available after start-up .
NetBotz 450/550/570 | Physical Description
- Status LED: blinks orange and green at start-up , then indicates the status of the network connection (solid green = ...
The use of non computer type loads with a UPS, specific to Back-UPS, Smart-UPS SC
Ensure that the Volt Amp rating of the UPS is sufficient to handle the start-up inrush current draw of the motor.
What are your condenser clearances and placement requirements?
Condensers also may require additional wiring to power the recive heaters, this can be reviewed upon start-up
Battery Discharge During Storage
Depending on the health of the batteries, they can discharge below start-up voltage (approximately 85vdc) within 72 hours if the ...
NetBotz 355 | Physical Description
- Status LED: blinks orange and green at start-up , then indicates the status of the network connection (solid green = ...
NetBotz 455 | Physical Description
- Status LED: blinks orange and green at start-up , then indicates the status of the network connection (solid green = ...
APC UPS Network Management Card (NMC) Compatibility Chart
When the card is installed after the UPS, however, a new Start-up service (WSTRTUP-VS1-a50) needs ...


결과 1 - 10 의 12

찾고 있는 내용을 찾을 수 없습니까?

기술 지원, 불만 사항에 대한 지원 등에 관한 정보를 얻으려면 고객팀에 문의하십시오.