자주 묻는 질문 찾아보기



Network Attached Storage Support for NetBotz Version 2 Monitoring Appliances
... 420's can store alert, sensor, and visual data persistently to a remote network drive (NAS) by integrating into an existing storage ...
Data Center Expert | Can not access DCE Virtual Machine after upgrade.
If StruxureWare is only provided with the default 18 gig worth of drive space, the system may not be able to reboot after an ...
Humidity Issues in IT Data Centers
* Tape drive operation - Humidity can dramatically affect a tape drive’s ability to read and write data.
AP8XXX Series Rack PDU Power Output Specifications (CAN & USB ports)
... 24VDC nominal (4.8 watts) 8 USB Port - (for USB drive to upgrade PDU firmware only) 100ma @ 5VDC ...
Changing a machine name that is accessed by PowerChute Business Edition
< drive letter>\User\<user name>\AppData\Local\VirtualStore\Program Fils\APC\PowerChute Business ...
PowerChute Personal Edition 3.X "has stopped working" on Windows Vista or Windows 7.
... the Arial fonts - font family from you system CD, system back-up drive , or back-up CD.
Upgrade Procedure for NetBotz Version 2 and 3 Appliances with Advanced View
... upgrade file from the NetBotz Support Web Site manually and save it to a local drive and upgrade from the local file.
Differences between ap7xxx and ap7xxxb Series Rack PDU's
ap7xxxb models utilize a command-line driven Serial/Telnet interface, opposed to the menu- driven style of the ap7xxx units:
How do I use the Network Management Card to retrieve Event, Data, and Config Files on an InRow.
6) Locate event.txt in your Documents and Settings folder on your C:\ drive .
How do I upgrade the firmware on my Dry Contact I/O SmartSlot Card (AP9613)?
... a "Device with Removable Storage" and show as a drive on your computer, similar to a flash drive .


결과 1 - 10 의 26

찾고 있는 내용을 찾을 수 없습니까?

기술 지원, 불만 사항에 대한 지원 등에 관한 정보를 얻으려면 고객팀에 문의하십시오.