자주 묻는 질문 찾아보기



Where can I view community resources and documentation for Data Center Operation?
Our community forum that covers the DCO product can be found in the SE Exchange site on the EcoStruxure IT Forum:
How to properly update an NetworkAIR FM NMC via XModem.
Note—this is the default high level user name and pass word; this may have been changed by site personnel.
Changing the Language of the Symmetra PowerView RM Display
... . Support for additional languages may be available on the CD or at the APC Web site (http://www.apc ...
Rack PDU 2G (AP8XXX) Network Port Sharing Information
The Reset /Reboot web page has many additional reset /reboot options for Rack PDU groups.These
About->Support menu option missing from AP8XXX series Rack PDU Web Interface on certain firmware versions
In the interim, this page can be accessed by manually changing the URL in the address bar.
NetBotz | Reformatting a Version 2 or 3 Appliance
... it is entered, you will see a message on the web page that says the following: Configuration reset requested (keeping basic network ...
How do I upgrade my SRT, XU, or XP Smart-UPS firmware using my Network Management Card?
Step 6 - Reboot your NMC: From the NMC Webpage "Contol" menu Go to "Network" then " Reset /Reboot"
What changes need to be made to accommodate 240 volts on the input to the Matrix-UPS?
The input voltage selector must be adjusted in order to accommodate the new voltage requirement. This process is outlined on page 10 of the .
Changing the language on the PowerView RM display (AP9215RM)
French, German, Italian, and Spanish are available on the enclosed CD or from the APC Support website .
Why isn't the time changing on my Network Management Card (NMC) when I change Daylight Saving Time (DST) settings?
Keep in mind the web interface is static. Reloading the page a few minutes later should reflect the new time.


결과 1 - 10 의 50

찾고 있는 내용을 찾을 수 없습니까?

기술 지원, 불만 사항에 대한 지원 등에 관한 정보를 얻으려면 고객팀에 문의하십시오.