{"searchBar":{"inputPlaceholder":"키워드로 검색 또는 질문","searchBtn":"검색","error":"검색할 키워드를 입력하십시오."}}
{}

브랜드

{"support":{"yesButton":"예","noButton":"아니오","feedback":{"title":"어떻게 개선할 수 있겠습니까?"},"submitButton":"제출","successMessage":"의견 주셔서 감사합니다.","title":"도움이 되었습니까?","feedbackPercentLabel":"의 사용자가 이 답변이 도움이 되었다고 응답했습니다.","captcha":{"error":"확인란을 선택하십시오"}}}
FAQ 검색

PowerChute Network Shutdown – Hosts fail to enter maintenance mode when vSphere Clustering Service (vCLS) is enabled

Issue:
PowerChute Network Shutdown – vSphere Clustering Service (vCLS) introduced in VMware vSphere 7.0 update 1 prevents hosts from entering maintenance mode since vCLS agent VMs cannot be shut down

Products:
PowerChute Network Shutdown v4.x

Environment:
VMware vSphere 7.0 update 1
vCenter Server Appliance 7.0 update 1

Cause:
vSphere 7.0.1 introduced a new feature called vSphere Cluster Services (vCLS) that allows DRS and HA to continue functioning even when vCenter Server is unavailable.

The issue occurs because there are 3 vCLS Agent VMs deployed in the cluster that cannot be powered off during the VM Shutdown step along with other User VMs. When vCenter Server detects that these VMs are powered off, it will automatically power them back on. Since these VMs remain powered on, the Hosts on which they reside cannot be placed into maintenance mode.

Solution:
Enable VM Prioritization and add all User VMs to a priority group except for the vCLS VMs. vCLS VMs are named vCLS (<number>).

Configure a 0 second duration for VM Shutdown and VM Startup for the Un-prioritized group. This ensures that the vCLS VMs will not be shut down or powered on by PowerChute.

Ensure that Delay Maintenance Mode is enabled.

Please follow the instructions in the attached PDF (vCLS_ScriptInstructions). Alternatively, if you are not using DRS, you can choose to disable vCLS permanently by following the instructions here - https://kb.vmware.com/s/article/80472

NOTE: If the vCLS VMs are added to a higher priority group than the vCenter Server Appliance VM, the scripts are not required to place the cluster into retreat mode. This is only applicable if vCenter is inside the cluster.

찾고 있는 것을 얻지 못했습니까?

다른 지원 툴로 빠른 지원을 받으십시오.