Browse FAQs



Data Center Expert | How can I resolve “Failed to create java virtual machine.” error when launching StruxureWare Data Center Expert client?
... Upon launching the StruxureWare Data Center Expert client an error ... StruxureWare Data Center Expert (DCE) ... - Standard Appliance (ap9470 ... StruxureWare Central (SWC ... StruxureWare Client (potentially ... StruxureWare may be attempting ... 1 ) Navigate to the Installation directory for StruxureWare Data Center Expert . (default directory is: C:\ Program Files (x86)\ StruxureWare Data Center Expert X.X.X) ... -vm "C:\ Program Files (x86)\ StruxureWare Data Center Expert 7.2.7\dcexpert\jre\bin\javaw.exe"
Data Center Expert | Why does StruxureWare not accept my One Time passcode?
StruxureWare Data Center Expert is not accepting ... StruxureWare Data Center Expert (DCE) ... - Standard Appliance (ap9470 ... StruxureWare Central (SWC ... StruxureWare Data Center Expert (all versions ... StruxureWare Central (all ... SturuxureWare Data Center Expert requires a 64 ... passcode and the Data Center Expert's MAC address. StruxureWare Data Center Expert (DCE) ... behave as a standard trap receiver. ... does not cause standard SNMP traps to ... ... to gather specific information about the alert ... 1 . In a ... AP9465 = StruxureWare Data Center Expert Basic ap9470 = StruxureWare Data Center Expert Standard
Data Center Expert | How do hardware and software support contracts work?
Cause: StruxureWare Data Center Expert appliances come with 2 years of factory hardware warranty and no
Is StruxureWare DCE or NetBotz vulnerable to CVE-2017-7494 (Samba related vulnerability)?
Are StruxureWare DCE or NetBotz ... StruxureWare Data Center Expert (DCE) ... - Standard Appliance (ap9470 ... StruxureWare Central (SWC ... StruxureWare Data Center Expert (all versions) StruxureWare Central (all versions) ... Experts say the vulnerability can be exploited with just one line of code and has the potential to spread quickly. Samba versions 3.5 (released March 1 , 2010) and onwards are impacted. ... StruxureWare DCE v7.X runs on Linux but does not export SMB shares, so it is not vulnerable. ... Cyber Security is an important element of Schneider Electrics' commitment to software quality.
Video: Data Center Operation | Copying files from the StruxureWare Data Center Operation
1 . Open the application 2. Enter IP address or hostname within the "Host Name" field
Why isn't my DNS change saving in StruxureWare Data Center Expert?
Changing DNS entries in StruxureWare Data Center Expert UI for VM does not save changes. ... StruxureWare Data Center Expert ... StruxureWare Data Center Expert VM with single NIC configured ... It has been seen where changing a DNS entry in StruxureWare Data Center Expert (DCE) when using the console application does not cause the system to reboot and save the DNS changes. This only happens on a system with a single NIC so it is not seen on the DCE hardware servers, only on a DCE VM server.
Data Center Expert | How do I enable SSL communication between StruxureWare and multiple Netbotz devices?
StruxureWare Data Center Expert (DCE) ... - Standard Appliance (ap9470 ... StruxureWare Central (SWC ... StruxureWare Data Center Expert (all versions ... StruxureWare Central (all ... Struxureware Data Center Expert and Netbotz Communication ... Struxureware Data Center Expert (SWDCE) ... received from any one Netbotz device. Information retrieved from each ... may include alarm data , configuration data , or surveillance data . ... will now POST information to the SWDCE ... alarm or other data . ... will show status information on all devices ... ... you can create one discovery for the ... ... /Post Alert Data Settings.
What is priority scanning in StruxureWare Data Center Expert?
StruxureWare Data Center Expert StruxureWare Data Center Expert 6.x ... ... NMC) version 1 and 2 StruxureWare Data Center Expert (DCE) ... ... alert state The information received is intended ... ... for their sensor data and current state ... ... on the retrieved information . StruxureWare Data Center Expert help defines priority ... ... at which the StruxureWare Data Center Expert server is defined ... Here is a little more information on the process: ... DCE receives the trap and then polls the device for alert information . The alert has now been verified and DCE will notify users based on their notification policy .
Can StruxureWare Data Center Expert output a 32 bit register with its Modbus output?
A single register in StruxureWare Data Center Expert's modbus output is ... StruxureWare Central / StruxureWare Data center Expert StruxureWare Central any version StruxureWare Data center Expert any version ... output of a single register for StruxureWare is a 16 ... ... handled by a single register. ... bit register in StruxureWare . ... this limitation, StruxureWare Data Center Expert can be configured ... StruxureWare does not know ... ... value of either 1 or 2. ... ... , the polling software must be reconfigured ... 31000 returns 0000000000000001 If this were a single register, = 1 ... This math must all done on the side of the querying application .


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.