In Hyper-V, Virtual Machine shutdown is delayed when VM Migration is enabled.
Published date:
05 October 2020
Issue:
There is a delay proceeding with virtual machine shutdown when VM migration is enabled for Hyper-V.
Product Line:
PowerChute Network Shutdown v3.1 up to v4.3
Environment:
Windows Hyper-V
Cause:
If the VM Migration time is insufficient in attempting to migrate all VMs, there is a timeout issue before PowerChute proceeds with shutting down VMs that failed to migrate.
Resolution:
Ensure you allow sufficient time for the VM migration duration to attempt to migrate all VMs.
NOTE: This is is resolved in PoewrChute Network Shutdown v4.4.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.