Browse FAQs

"Notify All Connected Users" not working in RHEL 6.3

Published date: 04 October 2019

Issue:
The "notify all connected users" function does not working in RHEL 6.3 (Red Hat Linux version 6.3)

Product Line:
PowerChute Business Edition

Environment:
OS: RHEL 6.3 X64
Build: PowerChute Business Edition 8.0.1 and 9.x OEM Basic

Cause:
Notifications are not sent to remote RHEL machines or other Windows machines in the same network.
Instead, notifications are seen only at the localhost, that is, the RHEL machine where PowerChute Business Edition is installed.

Notifications can be sent to Windows machines when this RHEL PowerChute Agent is added to a PowerChute Console.
These notifications are sent from the Console installed on Windows and not from RHEL.


Resolution:
This issue will be addressed in a future PowerChute Business Edition release.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.