Power
Uninterruptible Power Supply (UPS)
Surge Protection and Power Conditioning
Audio-Video Solutions
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
Data Center Containment
Power Distribution
Row 3 Phase Power Distribution
Rack Power Distribution
Room Power Distribution
Transfer Switches
Prefabricated Data Center Modules
Power Modules
IT Modules
DATA CENTER SOFTWARE
Monitoring & Control
Software Services
Modelling and Planning
Operations
Services
Install
Operate
Optimize
Renew
Product Based Services
View All Solutions
Business Solutions
Home Solutions
Get Support
Need Help? Start here
Product Documents & Software
Product Guides
Additional Links
Contact Us
Browse FAQs
Issue: PowerChute Personal Edition v3.0, 3.0.1, 3.0.2 : Installation says the Data Service failed to start Product Line: PowerChute Personal Edition (PCPE) version 3.0, 3.0.1, 3.0.2 Environment: All supported Windows OS Cause: This issue happens if you do not have the latest service pack of .Net 2.0. Solution:
1. Open up the Control Panel
2. Go to Programs and features
3. In the left panel select Turn Windows features on or off
4. From the list select Microsoft .NET Framework 3.5.x and then click ok. Windows will install the service NOTE: PCPE 3.1 requires .NET 4.0