Browse FAQs



Symmetra PX1-PX2; What happens when PX1, PX2 and 250/500k PX is EPO'd
Symmetra PX ... describes how the Symmetra PX reacts to ... ... , from a single point by activating ... ... circuit in the Symmetra PX is activated ... or in the XR Frame (80kw ... ... tripped on ISX PDU . There is no power on the output of the XR Battery Frames or on the output of the Symmetra PX UPS . ... Only the Battery CBs on XR frames will be tripped. Customer would need to have optional shut trip on Upstream CB to turn off input power to UPS . ... All Battery CBs on battery frames and Q 2 will be tripped ... Reset EPO switch and follow proper procedures to restart UPS
Mounting the Symmetra LX in a 2 post rack
How do I mount a Symmetra LX in a 2 post rack? ... Symmetra LX ... Symmetra LX ships with a 4 post rail kit only, however it is possible to safely mount the UPS system and any associated XR frames in a 2 post rack. ... ( 1 ) SYOPT12 must be purchased and used for each Symmetra LX mainframe or extended run ( XR ) battery frame that is to be mounted.
E3 error message on the Symmetra Extended Run Battery Frame (XR frame)
The XR frame of a single phase Symmetra displays E3 ... mainframe indicates an XR Frame Fault. Symmetra Power Array Symmetra RM Symmetra LX ... message on the Symmetra XR Frame is an ... communication between the Symmetra mainframe and the Symmetra Extended Run ( XR ) Battery Frame ... ... communication between the two frames where the Power ... located in the XR Frame. ... function of the UPS if it were ... ... that event the UPS goes on battery ... ... card on the Symmetra Extended Run Frame ... 1 ) Disconnect the ... back of the Symmetra Extended Run Battery ... 2 ) Disconnect the ...
Batteries discharged to a low voltage in a single phase Symmetra frame
Single phase Symmetra battery modules are ... Symmetra Power Array Symmetra RM Symmetra LX There are two possible causes of ... 1 .) If ... ... to place the UPS into a bypass ... 2 .) When ... installed in a Symmetra frame, it ... If the Symmetra is powered down ... ... to place the UPS into a bypass ... All Symmetra and Symmetra RM units ship ... : Symmetra LX was designed ... ... only applies to Symmetra Power Array and Symmetra RM. The Symmetra will not be ... ... modules in connected XR frames ).
Single Phase Symmetra XR Frame Compatibility
Issue Single Phase Symmetra XR frames are compatible only with certain UPS systems.
Symmetra Power Array reads "Bypass Out of Range"
Symmetra Power Array shows ... Symmetra Power Array ... This document describes one of the reasons ... a North American Symmetra Power Array may ... ... operation of a Symmetra Power Array, ... ... default, the Symmetra Power Array comes ... ... input of the Symmetra to a 240vac ... ... " of the Symmetra Main Intelligence Module ... ... (0's or 1's ). ... indicates whether the Symmetra's Input Voltage Jumper ... ... equal to " 1 ", then ... ... 4 in their Symmetra User's Manual. ... procedure, the UPS MUST be fully ... 1 . Turn the ... 2 . Turn off ... rear of the Symmetra .
How to change the Input Voltage Select Jumper on a Symmetra Power Array
... environment of my Symmetra Power Array and ... Symmetra Power Array Before the UPS is started up ... : UPS must be completely ... 1 . Switch the ... 2 . Open the ... front of the UPS . ... that feeds the UPS . 4. Remove all battery modules from the UPS . 5. Disconnect any extended run ( XR ) battery frames from the UPS . ... 1 . Refer to figure below. ... 2 . Use a small, flat head screwdriver to position the input voltage jumper to the correct voltage setting. ... 3. Replace the voltage select access panel and continue with connecting the UPS to utility power.
Things To Consider When Upgrading or Downgrading a Network Management Card 2 (NMC2) Device between v5.X.X and v6.X.X
Devices utilizing the Rack PDU 2 G app ( ... ), Smart UPS /Matrix application ... sumx) and Symmetra Single Phase (sy) ...
acdc1010 Hot Aisle Containment Rack Expansion Bundle Kit Installation (Manual)
... operation while the PDU , UPS , or XR Battery Cabinet is ... 1 . Never work ... 2 . Perform the ... ... electricity to the PDU , UPS , or XR Battery Cabinet, ... ... working on the PDU , UPS , or XR Battery Cabinet. ... requires at least two persons to safely ... ... from the equipment frames ... system, install two 21 U side ... ... , there are two PSX/ PDU side panel installation ... a PSX or PDU . ... next to a PDU or UPS , then a PSX/ PDU side panel ( ... installed on the PDU or UPS .
What is the maximum number of XR frames allowed with a Symmetra PX 20, 40 and 80kw solution?
Symmetra PX; What ... maximum number of XR frames allowed with a Symmetra PX solution? Symmetra PX 20, ... ... maximum number of XR frames allowed with a Symmetra PX solution is ... ... size of the Symmetra PX Main Frame ... For a Symmetra PX 20 or ... populated (Battery Frames ) XR frames . ... a runtime of 1 hr 40 mins ... ... of addresses for XR frames . ... a fully populated XR frame is SYCFXR8 ... ... consists of the XR frame with 8 ... ... this equals an XR frame with 32 ... For a Symmetra PX 80kw Frame ... 3 fully populated XR frames .


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.