Browse FAQs



DAC, Cancoil Installation Manual
Section 1 . Warranty and ... Section 4 . Leak Testing ... Section 1 . ... proper servicing and preventative maintenance . ... must be refrigeration grade only. ... equal to 2 degrees per 100 equivalent ... are based on 1 degree per 100 equivalent ... ... a rate of 1 ” drop per ... ... a rate of 1 ” drop per ... ... and should have 1 additional trap per ... Section 4 . Leak Testing ... ... the system with 1 / 4 ” minimum ID ... 1 . Check the ... 4 . Check the operating control settings. ... It is important to inspect each unit at start-up and before service or maintenance to determine which omponents have been installed.
What are some features I need to be aware of while manipulating the config.ini file of a APC Network Management Card?
... Network Management Card 1 (NMC1) ... ... Network Management Card 1 include (but ... file back on a network card, the override keyword MUST match the MAC address of the card for the four settings listed above to apply. ... On newer generation Micro -link UPS devices, such as SMX, SMT, SRT, and SURTD the following keywords in config.ini are protected by UPSOverride: ... These values are protected to avoid accidently setting the same potentially "site specific" settings to multiple UPSs without extra care , just as with the TCP/IP settings.
My Micro DC came with clamp-on ferrites. Where do they go, and are there installation instructions?
Cause: The Micro Data Center SX International units ship with one snap-on ferrite per piece of installed equipment.
What are the causes of premature motor failure in single-phase motors?
... motor failure in single -phase motors ... One of the most ... motor failure in single -phase motors ... ... Electric SA lead four training courses throughout ... to increase the level of expertise in ... Franklin Electric's single -phase motor ... ... fast; therefore care must be taken ... Step 1 : Number the wires 1 ; 2 & ... ... the wires ( 1 & 2) ( 1 & 3) ... a low ( 1 & 2) ... a high ( 1 & 3) ... ... per (Fig 1 )Understanding this ... ... start wire ( 1 & 3) ...
SRT 8 or 10kva reports Error P.11 or DC Bus Soft Start or event codes 124/125
The UPS reports P.11 or DC Bus Soft Start - event 124/125 ... 1 . Improved system performance of transitions between Online and Bypass operation modes. ... 3. Improved system behaviour to eliminate false detection of DC bus under voltage alarm under certain conditions. 4 . Improved system handling for certain AC input conditions during system start-up.
SRT 8 or 10kva reports Error P.11 or DC Bus Voltage Low or event codes 128/129
The UPS reports P.11 or DC Bus Voltage Low - event 128/129 ... 1 . Improved system performance of transitions between Online and Bypass operation modes. ... 3. Improved system behaviour to eliminate false detection of DC bus under voltage alarm under certain conditions. 4 . Improved system handling for certain AC input conditions during system start-up.


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.