Browse FAQs



ACSC1XX Spare Parts List
CAP MTL PPR 400v 5% 40uf RD (compressor) ... CONVERSION TO TOSHIBA COMP KIT , SC, 50hz - SPARE PART ... GROMMET RUBBER 1 1/2"ID X 1 3/4"GD X 1/8"GW (for power cable at the bottom)
DELETE-Symmetra PX 160kw Power Module
sypm10kh = 400v 10kw Power Module sypm10k16h = 400v 16/10kw Power Module
ACRP1XX, ACRD5XX, ACRP5XX, and ACRC5XX Parts List
- Spare Part w0w3107 Cable Main Power 208/ 400v For acrp100/102 (DX)
Symmetra RM running on battery with good Input Voltage
However, if the UPS is configured for 50hz +/- 3hz, then the UPS will subsequently run on battery power due to ...
What is the input voltage required for the InRow acrd100/200? Is a power cord supplied with the unit?
... unit uses a single phase 208v/60hz input in NAM and a 230v/ 50hz input in the rest of the world.
Can the NetShelter CX integral PDU be replaced, or can another be added if a dual power input is required for redundancy? Which PDU comes in the CX?
... PDU included with the cabinet is the APC part number AP9568 for EMEA cabinets ( 50hz ), and AP9567 for NEMA cabinets (60hz ...
Information on Online and On Battery operation of 3:1 Symmetra UPS systems
Symmetra Power Array ... When a Symmetra 3:1 is operating On-Line it is drawing balanced power from all 3 phases, i.e., it is drawing the same current from each of the 3 phases. ... The 3 phase power is fed to all the Power Modules where it is filtered and converted to single phase and sent to the output. ... When Symmetra 3:1 is On Battery it will provide single phase output power . ... The output frequency can also be set to either 50hz or 60hz.
Symmetra PX; Bypass not in Range messages
You can configure the output frequency on the Power View: ... 50hz +/- 0.1 Hz 50hz +/-3hz 50hz +/-10hz
Why is the UPS thermal dissipation rating calculated using efficiency data different from the value specified on www.apc.com?
The value calculated using efficiency data or the Efficiency Comparison Calculator is based on nominal environmental conditions (25C, 230v 50hz input), in green mode with a fully charged battery. The values on the web are specified for less-than-nominal environmental conditions, such as maximum charging power , active AVR, high ambient temperature, etc.
Can I use a domestic model UPS in a foreign country?
Different countries produce and utilize power in different ways. ... Most European countries utilize an input voltage of 230 volts at 50hz .


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.