Browse FAQs



Can the split rear doors of a NetShelter SX, SV or VX cabinet be installed on the front of the cabinet, and can the front door be installed on the rear?
Issue: Design of the data center may require a full width door on the rear and/or split doors on the front.
Can split doors be installed on the front of a NetShelter SX, VX or SV cabinet?
It can not be assumed that the rear split doors will install onto the front of the cabinet. Confirmation is needed.
Can the horizontal cable side channel organizer be installed into a 600mm wide NetShelter SX, VX or SV cabinet?
... mounting rails of NetShelter SX 750mm wide cabinets. NetShelter Cable Management ... from front to rear in a 600mm wide NetShelter cabinet. ... the narrower 600mm wide NetShelter cabinets when paired ... ... the front and rear of the cabinet ... Some customers installing the ar8603a in the front of the cabinet may notice that the cable manager will interfere with the door closing when the rails are in their forward most position. This issue can be overcome by installing the cable manager to the rear of the front rails so the cable fingers are facing inward.
What are the perforation pattern percentages of the NetShelter SX, SV or VX cabinet?
Some equipment manufacturers may request minimum perforation pattern percentages for the front and rear doors of an enclosure which houses their equipment.
Where are the Model and Serial numbers on the NetShelter SX, SV or VX?
The serial number and model number are located on a label inside the rear doors on the top of the frame.
Do NetShelter SX or SV cabinets in NAM have UL stickers? If so, where are they located?
On the SX cabinet the UL sticker is located on the lower rear frame. Simply open the rear doors and look down.
What spare parts are available for my NetShelter SX, VX, WX, AV, SV, Colocation, EP, ES, VS, 2-Post Rack, 4-Post Rack?
netshelter , part, ... , vx, sv , wx, ... ar1000, ar2800, door , doors , front, rear , roof, ...
acdc1010 Hot Aisle Containment Rack Expansion Bundle Kit Installation (Manual)
Door and Door Frame Removal The door frame is heavy ... ... you reinstall the door and door frame. ... to remove the door frame assembly from ... ... panels onto each NetShelter VS (900 ... mm) or NetShelter VX (1070 ... Rear joining brackets for ... ... When joining two NetShelter VX (1070 ... ... . Remove the rear doors of the enclosures ... Rear joining brackets for ... ... When joining two NetShelter VX (1070 ... Remove the rear doors of the enclosures ... ... to remove the rear doors . ... not remove the rear doors of the UPS ... ... . Use appropriate rear joining brackets.
Can the vertical cable management fingers for 600mm wide NetShelter cabinets be installed into 750mm wide NetShelter cabinets?
... AR7723 into a wide NetShelter SX or SV . NetShelter SX and SV ... compatible with the wide SX or SV cabinets. ... into a 750mm wide cabinet. ... for the 600mm wide NetShelter SX cabinets, ... with the 600mm wide cabinets only. In the SX cabinets a better choice may be the ar7580a ( 42U ), AR7585 (45U) or AR7588 (48U) because they offer far more capacity. In the SV cabinets AR7721 and AR7723 are currently the only finger-style vertical cable managers available.
Which keys are used with NetShelter cabinets and EcoAisle, and how customers can obtain them.
Replacement NetShelter key or additional ... NetShelter Cabinets, EcoAisle NetShelter Replacement Keys for SX, SV , AV, ... ... used for various NetShelter cabinets and how ... NetShelter SX, SV , AV & ... ... replacement key for NetShelter SX, AV ... VX front & rear door handles and side ... NetShelter WX: ar100 and ar100 HD please use Part 840-0103 as the replacement key & door handle kit. ... NetShelter CX: ... Please use Part 0H-0292-SE as the replacement keys for all NetShelter CX door locks. ... Key for the sliding door : 0J-870-26645.


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.