acdc1010 Hot Aisle Containment Rack Expansion Bundle Kit Installation (Manual)
... Rack Expansion Bundle Kit next to a ... When joining two NetShelter VX (1070-mm) enclosures: ... When joining two NetShelter VX (1070-mm) enclosures: ... When joining a NetShelter VS (900-mm) to a NetShelter VX (1070-mm) enclosure, use rear joining brackets and trim. ... The ceiling panels are configured in two different widths based on the size of the enclosures they span.. ... 3. Attach the plinth blocks to the enclosures, using four M8 × 25-mm screws