NetBotz 750 | Physical Description
Physical Description of the NetBotz 750 ... NetBotz version 5 ... NetBotz v5.X ... 4 Leak Rope ports Used for connecting a NetBotz Leak Rope Sensor (nbes0308). ... Third-party, dry-contact state sensors require the NetBotz Dry Contact Cable (nbes0304), and third party, 0-5 V sensors require the NetBotz 0-5 V sensor cable (nbes0305). ... 10 Wireless Sensor Coordinator USB Port with Wireless NetBotz USB Coordinator (nbwc100u) installed. ... 14 4- 20 mA Inputs Inputs for industry standard 4- 20 mA sensors.