Browse FAQs



When finger-style vertical cable managers are used in a 750mm wide NetShelter cabinet, is it possible to also block off the cable pass-thru openings in the mounting rails?
Using the finger-style vertical cable managers inside a NetShelter cabinet, designers need to know how to block hot air from recirculating through the rails . ... NetShelter SX ... When there are finger style cable managers installed inside the 750mm wide NetShelter cabinet, AR7714 must be used to prevent hot air recirculation. ... Without the finger-style vertical cable managers in place, ar7706 is used in the wide NetShelter cabinets. It's a brush strip style airflow management product that allows cables to pass through. It installs onto the vertical mounting rail .
Can the horizontal cable side channel organizer be installed into a 600mm wide NetShelter SX, VX or SV cabinet?
... install into the mounting rails of NetShelter SX 750mm wide cabinets. NetShelter Cable Management ... in a 600mm wide NetShelter cabinet. ... the narrower 600mm wide NetShelter cabinets when paired ... The ar8603a has two large brush - stripped sections that allow cables to feed through. ... Some customers installing the ar8603a in the front of the cabinet may notice that the cable manager will interfere with the door closing when the rails are in their forward most position. This issue can be overcome by installing the cable manager to the rear of the front rails so the cable fingers are facing inward.
Can the horizontal cable troughs ar8008blk and ar8016ablk be used in conjunction with vertical cable managers ar7580a, AR7585 and AR7588?
... cable troughs will mount to the rails when vertical cable ... NetShelter SX Wide cabinets, vertical ... All 750mm wide NetShelter SX cabinets: ar7580a ... ... troughs on the mounting rails of a 750mm wide NetShelter SX cabinet. ... use the roof brush strips AR7714 (5 ... ... populate one vertical mounting rail in the cabinet ... ... requires 6 roof brush strips . ... requires 6 roof brush strips . One set of AR7588 requires 6 roof brush strips . Note: the vertical mounting rails for 48U cabinets have 7 thru-holes but the AR7588 only has 6. The center thru-hole in the mounting rails is covered by the AR7588.
Are 23" mounting rails available for NetShelter SX cabinets?
For customers who already own a 42U 750mm wide SX cabinet with 19" mounting rails (ar3150 or ar3350) we offer sku ar7510 ...
What is the exact placement of the cutouts on NetShelter SX mounting rails?
netshelter , rail , hole, holes, pma, 42u, 45u ... 48u, 600 mm, 750 mm, 600mm, 750mm ,
Can the AR8125 NetShelter AV Sliding Shelf be installed into an SX cabinet?
The M6 screw is too wide to fit through the holes in the horizontal mounting rail .
What is the minimum distance required between mounting rails in a NetShelter SX cabinet when installing the AR7725?
Issue: Customers may want to know what distance is required between the NetShelter SX mounting rails to install the AR7725.
What's the vertical mounting rail depth for the NetShelter SX cabinets?
Issue: Customers need to know the adjustable depths of the NetShelter mounting rails .
Can the vertical cable management fingers for 600mm wide NetShelter cabinets be installed into 750mm wide NetShelter cabinets?
Issue: A customer may want to install the AR7721, AR7722 or AR7723 into a wide NetShelter SX or SV.


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.