Browse FAQs



Hardwiring to 120v, 208v, and 240v loads from a 208v/240v SmartUPS RT UPS
These two models are split phase ... ... RT is a single phase UPS with ... ... not two balanced 120 volt legs as ... ... output legs are 180 degrees out of ... ... To supply a 120 v load, ... 2 120 volt legs that are 180 degrees out of ... ... 240 v/ 120 v panel where ... 2 legs of 120 v and from ... 120 v Hot Leg ... Hot Leg ( 180 degrees out of phase from the 120 v leg) ... legs that are 120 degrees out of ... ... you must use one of our split ... ... 4 wire input and will output 2 balanced 120 v ...
APC Schneider Cooling Unit Identification
All Product models , all serial ... Model Model Model ... In-Row Model Model Model Model AFX 1 = 1 Bay ... Bay 06 ( 1 Bay) 08 ( 1 Bay) Model ... CM 003 ( 1 T) ... -230/ 1 /60 ... =277/ 1 /60 1 -5T ... 1 -3T ... Model ... -230/ 1 /60 ... =277/ 1 /60 Model ... CM 15 ( 1 T) ... =208/ 1 /60 ... =230/ 1 /60 ... =277/ 1 /60 Model
When multiple critical events occur, why does PowerChute Network Shutdown 3.0.1 not shut down using the shortest delay value in one of the events?
... of 300 seconds for event 1 and 120 seconds for event 2. If event 1 occurs first and ... shorter delay of 120 seconds.
USB Power Usage Guidelines for Netbotz
NetBotz USB Device Power Consumption The Sensor Pod 120 requires 1 point of power.
What are the basic troubleshooting steps for the Universal Transfer Switch model UTS6H?
The generator output is not 120 Vac/240 Vac single phase. This is not applicable to the UTS6H as it is 120vac Input ONLY.
What are the basic troubleshooting steps for the Universal Transfer Switch model uts10bi?
The generator output is not 120 Vac/240 Vac single phase. This is not applicable to the UTS6H as it is 120vac Input ONLY.
What are the basic troubleshooting steps for the Universal Transfer Switch model UTS6 / UTS6BI?
The generator output is not 120 Vac/240 Vac single phase. This is not applicable to the UTS6H as it is 120vac Input ONLY.
Why can't I use a domestic model APC UPS on a ship
Issue: In North America, one would expect to see approximately 120 volts when
Standard Lens Specifications for the WallBotz 500 & Camera Pod 120
Environment: NetBotz 500 / Camera pod 120 (Owl 1 pod only)


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.