Browse FAQs



APC Schneider Cooling Unit Identification
All Product models , all serial ... Model ... Expansion A= Air Cooled E= Air Cooled Model Model ... In-Row Model Model ... Main A= Air Cooled Model ... ) A= Air Cooled Model AFX 1 = 1 Bay ... Bay 06 ( 1 Bay) 08 ( 1 Bay) ... ) A= Air Cooled Model ... CM 003 ( 1 T) ... ) A= Air Cooled E= Air Cooled w/Multicool R= Air Cooled w/Remote ... ... -230/ 1 /60 ... =277/ 1 /60
Where can I get support for APC and MGE Products?
Additional Management Cards and Options Air Cooled Chillers
Carrier 30ra010-055 AquaSnap® Air-Cooled Chillers with ComfortLink™ Controls 50/60 Hz
Issue: Carrier 30ra010-055 AquaSnap® Air-Cooled Chillers with ComfortLink™ Controls 50/60 Hz
DAC, Cancoil Installation Manual
All Models Section 1 . Warranty and ... Air Cooled Condenser DAC Air Cooled Condensers For information ... Section 1 . Cancoil air-cooled condensers have been ... designed to provide years of reliable performance ... stable, efficient year round operation for ... ... be used if air-cooled quipment is located ... ... are based on 1 degree per 100 ... ... a rate of 1 ” drop per ... ... a rate of 1 ” drop per ... ... and should have 1 additional trap per ... Cancoil air-cooled condensers are available ... information regarding the model in question. ... the system with 1 /4” ... 1 . Check the supply voltage when the system is operating.
What is the RDU’s entering water temperature guidelines
All Product models , all serial numbers ... 1 . What range of Entering Water Temperature should be supplied for the system? ... Typically if you chilled water source is starting to exceed its target set point, the chiller will alarm and begin to inform you of the problem as well.
Whether to install a suction line drier or liquid line drier
All Air Cooled Units ... All Product models , all serial numbers ... Installing a suction line drier in an ACRP DX is a tight fit, but possible. The obvious benefit of a suction line filter drier is the added protection given the system if a burnout should occur. The filter will effectively prevent contamination resulting from the failure from traveling back through the suction line into the other parts of the system. This will minimize the contamination remaining in the system when the inoperative compressor is removed. With this said, it is preferred to put the drier in the suction line. If a technician cannot find a suitable suction line drier with replaceable cores to fit inside the ACRP, a liquid line drier would be fine. It is ok to use an additional liquid line drier with replaceable cores. This can be handy since a technician will have more room on the outside liquid line to install isolation valves to keep the downtime to a minimum when replacing cores. The ACRP uses Danfoss liquid line drier pn # 023z4581, 5/8" ODF SOLDER. You will need to find a small suction line filter drier. After the cleaning procedure is completed, recheck in approximately one to two weeks to ensure that the system condition and operation is completely satisfactory.
How to navigate through an Network Air FM unit display
—for air-cooled Modules with no ... Air-cooled Systems with no ... event to one of the output ... Provide a unique name for each ... ... an input in one of the following ... ... , Expansion Module 1 , or Expansion ... ... > Expansion Module 1 > Module Config ... ... > Expansion Module 1 > Module Config ... ... > Expansion Module 1 > Module Control ... Main > Setup > Module > Expansion Module 1 > Module Control > Reset Humidifier ... Main > Setup > Module > Expansion Module 1 > Module Control > Set Up Humidifier ... Humidifier Model . The steam-electrode humidifier can be set to one of three modes:
What are the operational conditions for an InRoom (Stulz) Unit
Frequency:60 Hz +/- 1 % ... Maximum equivalent length of piping between the cooling unit and the air cooled condenser: 60 m (200 ft)
Why do I need refrigerant traps in my piping?
All Air Cooled Cooling Units ... It is customary to reduce the riser by one pipe size to maintain velocities over 1000 ft/min. Figure 1 shows the proper method for reducing the pipe diameter for discharge risers. ... figure 1 ... , it is advised to always install a single trap at the base of the riser if the riser will be less than 20 feet. ... A: Schneider Electric does not require a discharge line muffler nor do we recommend one .


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.