Browse FAQs



APC Schneider Cooling Unit Identification
All Product models , all serial ... Model ... Expansion A= Air Cooled E= Air Cooled Model Model ... In-Row Model Model ... Main A= Air Cooled Model ... ) A= Air Cooled Model AFX 1 = 1 Bay ... Bay 06 ( 1 Bay) 08 ( 1 Bay) ... ) A= Air Cooled Model ... CM 003 ( 1 T) ... ) A= Air Cooled E= Air Cooled w/Multicool R= Air Cooled w/Remote ... ... -230/ 1 /60 ... =277/ 1 /60
Where can I get support for APC and MGE Products?
Air Cooled Chillers ... Planning Tools and Publications ... Service Plans
Schneider Electric's Technical Support Policy for Older Versions of PowerChute Software
... far beyond this stated commitment, but this 1 - year policy is stated here so customers may take it into account for planning purposes ...
Single Phase Symmetra Extended Run (XR) Frame Cable Lengths
This information can be relevant if a user is planning on installing the products in slightly different areas - different racks, for example.
Steps to take when moving a Symmetra Power Array from one location to another
... case you need to either send any components back to the APC or if you plan on moving your UPS in the future.
DAC, Cancoil Installation Manual
All Models Section 1 . Warranty and ... Air Cooled Condenser DAC Air Cooled Condensers For information ... Section 1 . Cancoil air-cooled condensers have been ... designed to provide years of reliable performance ... stable, efficient year round operation for ... ... be used if air-cooled quipment is located ... ... are based on 1 degree per 100 ... ... a rate of 1 ” drop per ... ... a rate of 1 ” drop per ... ... and should have 1 additional trap per ... Cancoil air-cooled condensers are available ... information regarding the model in question. ... the system with 1 /4” ... 1 . Check the supply voltage when the system is operating.
3 Phase Products Service Level Agreements; Definition of coverage as relates to the service level agreements offered by SE
1 Annual PM Visit ... UPS & PDU Advantage Prime : See attached file; ARUO-ACQGSD_R7_EN_Advantage Prime ... 1 Annual Preventive Maintenance Visit ... 1 Annual Preventive Maintenance Visit 1 Set of air filters if applicable
What is the RDU’s entering water temperature guidelines
All Product models , all serial numbers ... 1 . What range of Entering Water Temperature should be supplied for the system? ... Typically if you chilled water source is starting to exceed its target set point, the chiller will alarm and begin to inform you of the problem as well.
UPDATED MARCH-2016: Unable to access my APC Network Management Card (NMC) enabled device via HTTPS (SSL/TLS)
... Network Management Card 1 (NMC1) ... ... Network Management Card 1 include (but ... ... who uses any one of the products ... One such example is ... ... future firmware update plans to address this ... ... Network Management Card 1 (NMC1) ... Automatic Transfer Switch models except ... a value of 1 to allow fallback ... Network Management Card 1 (NMC1) Information Bulletin: Effects of Microsoft Internet Explorer and other web browsers blocking key lengths less than 1024 bits​(blocking key lengths less than 1024 bits)
Whether to install a suction line drier or liquid line drier
All Air Cooled Units ... All Product models , all serial numbers ... Installing a suction line drier in an ACRP DX is a tight fit, but possible. The obvious benefit of a suction line filter drier is the added protection given the system if a burnout should occur. The filter will effectively prevent contamination resulting from the failure from traveling back through the suction line into the other parts of the system. This will minimize the contamination remaining in the system when the inoperative compressor is removed. With this said, it is preferred to put the drier in the suction line. If a technician cannot find a suitable suction line drier with replaceable cores to fit inside the ACRP, a liquid line drier would be fine. It is ok to use an additional liquid line drier with replaceable cores. This can be handy since a technician will have more room on the outside liquid line to install isolation valves to keep the downtime to a minimum when replacing cores. The ACRP uses Danfoss liquid line drier pn # 023z4581, 5/8" ODF SOLDER. You will need to find a small suction line filter drier. After the cleaning procedure is completed, recheck in approximately one to two weeks to ensure that the system condition and operation is completely satisfactory.


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.