Browse FAQs



Where can I get support for APC and MGE Products?
... 6 0034- 1 0034-100 ... 2M- 1 E 0035nd-3M- 1 E 0039- ... ... 2M- 1 E 0088nd-3M- 1 E 0100- ... 2M- 1 E 0226- ... 3 0377- 1 M 0377- ... ... 2M- 1 E 0719- ... 7 0859- 1 0859-10 ... ... 15M 12000- 1 M 12000- ... 15M 12008- 1 M 12008- ... 15M 12012- 1 M-E ...
Schneider Electric's Technical Support Policy for Older Versions of PowerChute Software
PowerChute Plus ... When new versions of software are released, Schneider Electric will continue to provide full technical support to customers for the previous version for a minimum of 1 year after the new version is released. In practice, Schneider Electric typically goes far beyond this stated commitment, but this 1 - year policy is stated here so customers may take it into account for planning purposes. ... PowerChute Plus (PC+) was discontinued March 2007
APC Schneider Cooling Unit Identification
All Product models , all serial ... Model Model Model ... In-Row Model Model Model Model AFX 1 = 1 Bay ... Bay 06 ( 1 Bay) 08 ( 1 Bay) Model ... CM 003 ( 1 T) ... -230/ 1 /60 ... =277/ 1 /60 1 -5T ... 1 -3T ... Model ... -230/ 1 /60 ... =277/ 1 /60 Model ... CM 15 ( 1 T) ... =208/ 1 /60 ... =230/ 1 /60 ... =277/ 1 /60 Model
What are the Dynamic Load ratings and Shipping Load ratings for NetShelter CX cabinets?
Persons planning data centers need ... Static Load Weight Rating is the maximum weight of the cabinet, plus installed equipment (with the feet locked), in it's final location. ... This is the maximum allowable weight of equipment installed in the cabinet during movement from one location to another within the same data center. ... Example: a customer who wishes to move a cabinet from one row to another in a data center must remove equipment until the weight is equal to (or below) the Dynamic Load Rating before being moved.
How can I adjust the number of battery packs on a Smart-UPS XL?
To adjust the number of battery packs via a Terminal session: 1 . Unload the PowerChute plus NLM (pwrchute.nlm)
RFC1628 MIB Compatibility with UPS Network Management Card 2 (ap9630/AP9631/AP9635)
... are named by an autonomous OID, upsAlarmDescr, to allow a single table to reflect well known alarms plus alarms defined by a particular ...
USB Specifications for the WallBotz 500
WallBotz 500 USB Specifications Range over fiber cable = 500 meters Plus 5 m at each end for total 510 meters ( 1 ,673 feet)
What does the Force Negotiation setting achieve in the Network Management Card?
... low, tells the NMC to increase values in # 1 and #2 below to the PCNS shutdown required time plus 70 seconds.
PowerChute Personal Edition v3.X Error Code 2738 – Unable to install the software.
Considering that, plus the fact that SFC /scannow is ... use, the tool should usually be one of your first troubleshooting steps.
UPS Performs Continuous Self Tests for One Hour Before Its Scheduled Time
Environment PowerChute Plus running on Netware 5 SP 3


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.