Browse FAQs



3 Phase Products Service Level Agreements; Definition of coverage as relates to the service level agreements offered by SE
Definition of coverages as relates to the service level agreements offered by SE UPS & PDU On-Site Warranty Extension :
Which SmartSlot accessories are supported by the Galaxy 3500 (g3500) UPS?
... supported by the Galaxy 3500 (g3500) UPS ? ... Facility 3 Phase UPS MGE Galaxy 3500 models ... supported by the Galaxy 3500 UPS (g3500) ... ... with the g3500 UPS . ... with the g3500 UPS . ... inputs, ( 1 ) output per ... AP9622 product page ... in the g3500 UPS . ... in the g3500 UPS . ... front panel/ UPS door will not ... 1 .) Purchase ... ... an APC ap9600 single slot SmartSlot expansion chassis and extend the cable to ... ... top of the UPS . ... SmartSlot in the UPS frame. ... top of the UPS .
How to take the Single Galaxy 5000 UPS from normal operation to total power off using an external Maintenance Bypass Panel
Cause: Due to site maintenance, inclement weather, and other conditions, request come in for assistance with Powering Down the Galaxy 5000 UPS
Video: How to take the Galaxy 5000 UPS from normal operation to total power off?
... Down the MGE Galaxy 5000 UPS Galaxy 5000, Galaxy 5500 Due to site maintenance, inclement ... Powering Down the Galaxy 5000 UPS ... power down the UPS are available on ... ... is for a single UPS without an external ... Step 1 : Touch any ... Step 4: Choose “Stop the UPS ” ... At this point, the load is no longer protected by the UPS . ... The UPS is now fully isolated from the load. ... Step 6: Turn the Q 1 Switch to Off ... There is still stored energy in the capacitors, and batteries inside the UPS . Never remove any covers or panels.
Which modular batteries can be used with the Galaxy VS All in One (AIO) model?
... used in the Galaxy VS All in One (AIO) ... Galaxy VS All in One Galaxy VS AIO model ... ... battery frames for extended run time. Wide Frame UPS , Tall Frame UPS , and Modular ... UPS will stay in ... Narrow Frame UPS : UPS will stay in ... UPS will stay in ... ... batteries into a UPS . GVSBTU Galaxy VS 7 Ah ... Modular Battery ( single module) GVSBT4 Galaxy VS 7 Ah ... GVSBTHU Galaxy VS 9 Ah ... Capacity Battery ( single module) GVSBTH4 Galaxy VS 9 Ah Smart High Capacity Battery String (4 modules) ... Install the proper rated batteries into the UPS . Confirm battery types are not mixed.
Video: How to take the Galaxy 5000 UPS from total power off to normal operation.
This procedure is for a single UPS without an external bypass panel.
Galaxy VM Seismic Certification and Anchoring Requirements.
Galaxy VM Seismic Certification ... Galaxy VM ... for documentation regarding Galaxy VM Seismic Certification ... ... to installation and site preparation work. ... the Schneider Electric website . Galaxy VM Product Home ... ... -supply- ups -/data ... -phase- ups / galaxy -vm/ ... Galaxy VM- 2012 ... Galaxy VM OSHPD pre ... ... -SA- Galaxy VM Typical Seismic ... ... 9GN8T9_R 1 _EN/ Galaxy VM Installation Manual: ... Galaxy VM Seismic Anchoring Document: BYSN-9GN8T9_R 1 _EN Galaxy VM Seismic Certification Document: COCR-9X4HHB_R0_EN
MGE STS, Galaxy 3000, 4000, 5000 and Galaxy PW; Wiring information for egx100 to any 66061-supported products
... – STS, Galaxy 3000, 4000, 5000 and Galaxy PW ... – STS, Galaxy 3000, 4000, 5000 and Galaxy PW ... , N and 1 . Slave address is 1 and wiring is ... ... This assumes only one 66061 card or UPS or STS is ... ... configured at the site . One is down ( ... ... required on the UPS /STS. The male DB9 connector is not supplied with the UPS but a black terminal block is supplied with the EGX.
Does the NTP need to be configured on the Galaxy VS internal NMC and the optional AP9644 NMC for all parallel or single Galaxy VS?
Resolution: Ensure that only one network management interface in the entire UPS system ( single or parallel) is set to synchronize time.


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.