Browse FAQs



DAC, Cancoil Installation Manual
All Models Section 1 . Warranty and ... Section 1 . ... be refrigeration grade only . ... are based on 1 degree per 100 ... ... a rate of 1 ” drop per ... ... a rate of 1 ” drop per ... ... and should have 1 additional trap per ... ... information regarding the model in question. ... high affinity for water . ... the system with 1 /4” ... 1 . Check the supply voltage when the system is operating. ... The following paragraphs describe the function and adjustment of the various components .Cancoil ... The ambient fan cycling controls will maintain a condensing temperature of about 115 degrees whenever the outdoor temperatures are greater than the values shown above.
UPDATED MARCH-2016: Unable to access my APC Network Management Card (NMC) enabled device via HTTPS (SSL/TLS)
... There are two parts to this issue ... One such vulnerability is ... ... Network Management Card 1 (NMC1) ... ... Network Management Card 1 include (but ... ... ACSCXXX, RACSCXXX Cooling Units (except ... acrc301h, acrc301s Cooling Units, ... who uses any one of the products ... One such example is ... ... Network Management Card 1 (NMC1) ... acrc ACRCXXXX InRow Chilled Water (except ACRC3XXX ... ... your local APC Cooling Support team) ... Automatic Transfer Switch models except ... your local APC Cooling Support team) ... ... your local APC Cooling Support team) ... ... your local APC Cooling Support team) ...
How to navigate through an Network Air FM unit display
... MultiCool® ( chilled water ) and DX ... ... , then the cooling setpoint is used ... ... the System is part of a redundant ... ... work as a single System. Water ... Half capacity uses one compressor and half ... ... avoid over- cooling while dehumidifying. ... the modes ( cooling , reheat, ... ... compressor (stage 1 ) in a ... ... for fluid- cooled options ... of fluid- cooled option. ... (glycol or water ) flow to ... ... will switch the cool or dehumidify mode ... ... —for the water or glycol line ...
acpa4000 Spare Parts List
Parts Please contact Cooling Tech Support to ... ... ROTARY 115/ 1 /60 ( ... ... (CAT2P16S3R126B- 1 A) ... (this pump only ... this with the water sensor pn# ... ... Fan (fan only ... BYPASS ADRI- 1 - 1 _4- ... ... Assy (fan only ... BULKHEAD MOUNT ( single float ... (az2280- 1 C-120a ... ... SPORLAN BBIVE- 1 -cp100- ... (BBIVE- 1 -cp100- ... ... TUBE TWIN INSERT 1 /8" ... ... 875-0853 Water Carry-Over ... 0M-0844 Water Sensor Kit For acpa4000 ... 1 Year Extended Warranty for NetworkAir acpa4000 (WEXTWAR1YR-AX-12)
Refrigerant charging table for a Uniflair Unit
... refrigerant lines/ chilled water piping are free ... ... made by brazing only ; do not ... Charging and maintaining the refrigeration circuit must only be performed by qualified personnel. ... 1 . Open any shut-off valves present in the system to ensure that all of the components will be tested. ... 1 . Open any shut-off valves present in the system to ensure that all of the components will be evacuated. ... Charge r410a as a liquid only . ... If the system is not ready for commissioning, then apply only a holding charge and record the amount charged.
APC Schneider Cooling Unit Identification
APC Cooling Unit identification. All Cooling Units. All Product models , all serial ... ... FM Air/ Water /Glycol Model W= Water Cooled F= Water Cooled D= Water Cooled ... G= Glycol Cooled ... B= Glycol Cooled ... P= Glycol Cooled ... W= Hot Water Model ... coil C= Chilled Water Model C= Chilled Water ... In-Row Model ... Main C= Chilled Water Model W= Water Cooled ... G= Glycol Cooled BA=208 ... Model W= Water Cooled ... G= Glycol Cooled Model AFX 1 = 1 Bay
Water leak in DataCenter.
... you find a Water leak on Indoor ... All DataCenter Cooling Units. All Product models , all serial ... ... , flush with water , or blow ... One of the very ... pour scalding hot water into it. ... consistently downward and only has one trap. ... also cause the water to back- ... it doesn't have one . and is thawing, it may run water from nearly any place. ... section where it is explained in great detail. ... clogs may cause the condensation water from the air conditioner to back up and overflow. Use the hot water tip above to clear it.
What's the difference between seismic Zone 4 maps and High Seismic Area maps? Can one be substituted for the other? Which cabinet should I choose?
... -0- 1 -2- ... ... , 0, 1 , 2, ... ... ) is the only building code that ... ... .S. model building codes, ... ... numbered 0, 1 , 2, ... ( 1 ) A single map cannot properly ... ... less contrast from one part of the country ... ... short buildings from one part of the country ... ... states to provide greater safety, less contrast from one part of the state ... ... the UBC took one of those two ... ... removal of zone 1 in eastern Washington ... ... of the UBC 1994 map can be found as one of the illustrations ...
ACRP1XX, ACRD5XX, ACRP5XX, and ACRC5XX Parts List
... a list of parts for a ACRP1XX ... before placing a parts order, as ... Parts . Please contact Cooling Tech Support to ... ... 0521 ADPTR ELBOW 1 /2 INCH ... ) [ PART OF SHIP LOOSE ... ... 61194 ADPTR STRAIGHT 1 /2 INCH - 1 /2 INCH ... Connections) [ PART OF SHIP LOOSE ... ... 0991 ADPTR STRAIGHT 1 /2 INCH ... MM PEX [ PART OF SHIP LOOSE ... PART OF SHIP LOOSE ... ... CABLE ATS # 1 200-240v ... CABLE ATS # 1 480v 0w3122 CABLE ... ) [ PART OF SHIP LOOSE ... ... 8MM ROHS [ PART OF SHIP LOOSE ...
How to read a pressure temperature chart for super-heat and sub-cooling calculations
... and sub- cooling calculations. All DX Cooling units. Single - component refrigerants and azeotropes ... and condense at one temperature for a ... Therefore, only one column is needed ... (see Figure 1 ) ... , more of one component will transfer to ... ... of temperature from one side of the ... ... defined by a single pressure-temperature ... ... each temperature: one for the saturated ... ... liquid pressures are only separated by 1 or 2 psi ... ... PT charts will only list one column for these ... ... higher glide ( greater than 5° ... ... as for a single - component refrigerant.


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.