How to navigate through an Network Air FM unit display
... the System is part of a redundant ... ... work as a single System. ... Half capacity uses one compressor and half ... ... compressor (stage 1 ) in a ... ... using chilled water only ). βfor air-cooled Modules with no ... Air-cooled Systems with no ... event to one of the output ... Provide a unique name for each ... ... an input in one of the following ... ... , Expansion Module 1 , or Expansion ... ... valve, map only the Econ ... > Expansion Module 1 > Module Config ... ... > Expansion Module 1 > Module Config ... Only