# cd tmp/pcbe911/
# ls
Linuxreadme.txt Linuxreadme.txt.ja_UTF8 rpms
Linuxreadme.txt.ja install_pbeagent_linux.sh
#./install_pbeagent_linux.sh
== PowerChute Business Edition Agent Installation ==
For instructions on upgrading PowerChute, please refer to the readme
file in the Linux install folder.
Different monitoring ports are available on the back of the UPS depending on
the UPS model.
Please select the appropriate option below to proceed with the installation
process.
What type of UPS monitoring port is on the back of your UPS ?