FAQの参照



NetBotz 450/550/570 | Physical Description
... NetBotz 450/ 550 /570. ... - Rack Monitor 550 (551) 1 AC line inlet ... - Flashing one very four seconds ... ... mA) to one connected device. ... Relay Outputs ports 1 ,2 Used ... 9 4-20 ... ... Used for connecting APC by Schneider Electric ... nbrk0450/ 550 - 5/ ... Enable the USB -to- ... 17 USB Type A ports (2 or 4) Used to connect USB devices to the appliance. The nbrk0550 and nbrk0450 have two USB ports, while the nbrk0570 has four. ... The complete NetBotz 450/ 550 /570 Installation and Configuration Manual can be found .
NetBotz TFTP upgrade/recovery procedure
... , 450, 550 , 570. ... procedure are the USB console cable and ... 1 ) Download the ... recent firmware from apc .com for ... , 450, 550 , or 570 ... ... ) Connect a USB cable from your ... ... will be a USB Serial port with ... If the USB Serial Adapter is ... ... Stop Bits: 1 1 ) Under Session ... 1 ) Type a ... ... ALL of step 9 before continuing. 9 ) Unplug the ... ... starting with step 9 ) Log into the appliance using a username/password of root/ apc to set the new root password and network settings on the appliance.
NetBotz 750 | Physical Description
1 AC line inlet ... 2 Switched Outlet Provides power to ... ... connected to this outlet , and the outlet may be configured ... ... Used to connect APC by Schneider Electric ... 9 Private LAN Provides a 10/100/1000 connection to a private local area network and 48 VDC to an attached device. 10 Wireless Sensor Coordinator USB Port with Wireless NetBotz USB Coordinator (nbwc100u) installed. ... 11 USB Type A Ports Reserved for future use. ... 13 Voltage Output Provides 12 VDC or 24 VDC (75 mA) to one connected device.
NetBotz 300-500 Series | Password reset procedure
... (nbrk0450/ 1 ), 550 (nbrk0550) ... 1 ) Locate the reset switch on the appliance. On a wall mount version (355/455) the reset button is on the bottom next to the USB -B port. On a Rack Mount appliance (450/ 550 /570) the reset button is next to the Input Power connection. ... • User ID: apc • Password: apc ... • Password: apc 4. Once you have logged in to Advanced View, change the root password and apc account password to ensure security.
Data Center Expert | Discovering a NetBotz 300-500 Series Appliance
NetBotz v3 Rack Appliance: 450/451 (nbrk0450/ 1 ), 550 (nbrk0550), & 570 (nbrk0570) ... APC Device: snmpv1 APC Device: snmpv3 ... 1 ) Log into the DCE Desktop Client using an Administrator account. ... 9 ) Select the Device Group to discover the NetBotz Appliance into and then click Next. ... 1 ) Log into DCE's web interface and click on Status in the upper-right. ... 9 ) Under Appliance Settings, double-click on Web Server.
NetBotz v3 | How do I configure network settings?
... (nbrk0450/ 1 ), 550 (nbrk0550) ... ... Appliance, select one of the configuration ... Configuration Option 1 - DHCP 1 ) Power on ... 1 ) Download and ... ... , skip step 1 . ... ) Connect the USB Cable between the ... ... will be a USB Serial Port, ... ... is not a USB Serial Port listed ... ... installed in step 1 . 1 ) Connect the USB Cable between the ... ... will be a USB Serial Port, ... ... is not a USB Serial Port listed ... Stop Bits: 1 ... and a password of apc ... 1 ) Download and install the Advanced View Application. ... If Advanced View is already installed, skip step 1 .
NetBotz 250 | Physical Description
Ports for the handle sensors (NBHN125 or NBHN1356) on doors # 1 and #2. ... 6 Universal Sensor ports Used to connect APC by Schneider Electric sensors and third-party dry contact sensors. ... 7 USB Port Used to connect USB devices to the appliance. ... 9 10/100 Network Port Provides the connection to the network.
Downloading the MIB file for version 3 Netbotz.
NetBotz v3 Rack Appliance: 450/451 (nbrk0450/ 1 ), 550 (nbrk0550), & 570 (nbrk0570) ... The latest MIB should also be available on the APC software downloads page at: http://www. apc .com/tools/download
NetBotz 250 | Configuring Network Settings
1 ) Navigate to ... :// apc .com/ ... 1 ) Select a USB port at the ... ... Connect the provided USB A- USB mini B configuration ... ... no parity, 1 stop bit, ... ... -to- USB vritual COM port ... ... 5) Use apc for the user ... ... ) Use this one -line command ... 1 ) Use the ... ... b7 63 9 f 67 as ... address, use one of the following ... ... -63- 9 f-67 ... :63: 9 f:67 ... defined in step 1 , use one of the following ...
NetBotz v3 | Security Information
NetBotz v3 (355,450, 455, 550 , & 570) ... Manual created user and password (default apc / apc ) Authentication server integration support. ... - If SNMP is required, consider changing the V 1 community strings, and do not user snmpv1 thereafter.


結果 1 - 10 の 50

目的の情報が見つかりませんか?

カスタマーチームにお問い合わせいただき、テクニカルサポート情報、クレームへの対応、その他のサポートを受けることができます。