FAQの参照



Data Center Expert | How do I update incorrect UPS battery ages?
Battery Age for UPS ... ... Expert polls the battery age from each ... ... accurately display the battery age. The Battery Age report within StruxureWare DCE may report unknown values if the battery age is not set correctly. Updating the Last Battery Replacement Date on NMC Firmware version 6 .X and newer 1 ) Log into the UPSs web interface. ... 3) Set the Last Battery Replacement ... Updating the Last Battery Replacement date on NMC Firmware Version 5.X and lower 1 ) Log into the UPSs web interface. ... 3) Set the Last Battery Replacement date
NetBotz | Hardware & Software Support Information and Limits
Year 1 Year 2 Year ... Year 5 Year 6 Software Support & ... as wireless sensor batteries (covered under ... Year 1 Year 2 Year ... Year 5 Year 6 Software Support & ... as wireless sensor batteries (covered under ... Year 1 Year 2 Year ... Year 5 Year 6 Software Support Out ... ... as wireless sensor batteries (covered under ... Year 1 Year 2 Year 3 Year 4 Year 5 Year 6 Software Support Out of Support Hardware Support Factory Warranty Out of Support
Can I change the individual batteries inside of a Smart-UPS replacement battery cartridge?
All of these components are designed with a duty cycle equivalent to one battery life cycle.
NetBotz 750 | What parts come with the NetBotz 750?
... 8 m ( 6 ft) 1 10 NEMA 5 ... 8 m ( 6 ft) 1 11 USB- ... 2 m ( 6 ft) 1 12 A-Link Terminator 1
NetBotz 250 | Configuring Network Settings
6 ) Use this one -line command to configure network settings (text in italics indicates a variable that needs to be entered in ...
Wireless Sensor Pod 180 connected via AC-USB adapter may function as an End Device
1 . A Wireless Sensor Pod 180 powered by batteries joined the network in End Device mode.
NetBotz 750 | Configuring Network Settings
6 ) Configure your appliance to use network settings ... mask, gateway address, and at least one IP address for a DNS server.
Video: Data Center Expert | Desktop Client Requirements, Download, & Installation
A PC with a 1 -GHz or better AMD/Intel processor running ... ® Enterprise Linux® version 6.0; CentOS 6
Data Center Expert | Enabling SSH
1 ) Log into the DCE Desktop Client using administrator credentials. ... The appliance will restart some services during this time. ... 1 ) Connect to the Data Center Expert console: ... 6 ) Enter through the rest of the questions, as the defaults should be what was previously set on the appliance. ... If the values are blank or not correct, enter the correct ones for each question.
Data Center Expert | Downloading Log Files for Technical Support
1 ) Open a Web Browser and Navigate to: http://DCE_IP/capturelogs ... 4) Click on Create Service Log Archive. ... 6 ) Provide to technical support for analysis of your issue.


結果 1 - 10 の 50

目的の情報が見つかりませんか?

カスタマーチームにお問い合わせいただき、テクニカルサポート情報、クレームへの対応、その他のサポートを受けることができます。